Skip to main content
RAyub.1
Visitor II
February 10, 2020
Solved

Can I use Induction motor for STEVAL-IHM028V2 kit?

  • February 10, 2020
  • 3 replies
  • 766 views

I have a door project that is using 230V 3 phase Induction motor. I purchase STEVAL-IHM028V2 kit and STM3241G-EVAL for testing. I'm new in STM32 programming.

This topic has been closed for replies.
Best answer by Laurent Ca...

Dear @RAyub.1​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards

3 replies

Laurent Ca...
Senior III
September 11, 2020

Dear RAyub.1

Do you have still this problem to solve?

Best regards

Laurent Ca...

Laurent Ca...
Senior III
September 23, 2020

Dear @RAyub.1​ 

I guess you don't have to solve this problem anymore, therefore I consider this post closed.

If not, feel free to reopen it by posting a new answer.

Best regards

Laurent Ca...

Laurent Ca...
Laurent Ca...Best answer
Senior III
June 28, 2021

Dear @RAyub.1​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards