Receiving wrong Data in UART in Nucleo Board.
Hi, I was testing UART communication using F446RE Nucleo Board. I was sending data to COM port by a python program running in PC and trying the receive to same data.
ser.write(serial.to_bytes([1, 2, 3, 4, 5, 6, 7, 8, 9, 10, 11, 12, 13, 14, 15]))
print(ser.read(15))memset(rx_buffer,0, 15);
HAL_UART_Receive(&huart2,rx_buffer, 15, HAL_MAX_DELAY);
HAL_UART_Transmit(&huart2,rx_buffer, 15, HAL_MAX_DELAY);I'm getting below data.
b'\x01\x02\x03\x04\x05\x06\x07\x08\t\n\x0b\x0c\r\x0e\x0f'I tried same code in two different board. both are giving same result.