Skip to main content
AShva.1
Associate III
Feb 9, 2020 11:12 AM UTC
Solved

Can't open /dev/ttyRPMSG0 :(

I'm trying execution code:

#define DEVICE "/dev/ttyRPMSG0"
 
int main(void)
{
 int fd;
 struct termios tty;
 char buf[100];
 int len;
 
 printf("Opening device...\n");
 fd = open( DEVICE, O_RDWR | O_NOCTTY | O_NDELAY ); // read/write, no console, no delay
 if ( fd < 0 )
 {
 printf("Error, cannot open device\n");
 return 1;
 }
}

But, always get: Error, cannot open device. :(

I think, that in my Linux system there is no driver for this device: /dev/ttyRPMSG0.

What am I doing wrong?

How to create and manage a device /dev/ttyRPMSG0 from a program correctly?

Board: STM32MP157C-DK2

Many thanks.

This topic has been closed for replies.
nick67
nick67Best answer
Associate
Feb 9, 2020 12:34 PM UTC

Hi AShva.1,

let me share with you the two projects attached to this message (they are compressed in a single zip file).

One runs on Cortex-A7 and the other on Cortex-M4.

Virtual UART is created in Cortex-M4 project, in the main.c file.

0690X00000D8vfEQAR.png

Then, in Cortex-M7 project you can find the connection from A7 processor to the Virtual UART created before from M4 processor:

0690X00000D8vfYQAR.png

The full application aims to build a user interface on the LCD touch screen via GtkBuilder on Cortex-A7.

Then you'll obtain three graphic buttons that, once pressed, send a message through IPCC to the Cortex-M4.

This one receives the message, decode it and toggles the related LED:

0690X00000D8vg2QAB.png

Please note that in this project first the Cortex-M4 has to create the virtual UART and then the Cortex-A7 can connect to this UART.

Hope it could be useful.

Regards

Nicola

8 replies

nick67
nick67Best answer
Associate
Feb 9, 2020 12:34 PM UTC

Hi AShva.1,

let me share with you the two projects attached to this message (they are compressed in a single zip file).

One runs on Cortex-A7 and the other on Cortex-M4.

Virtual UART is created in Cortex-M4 project, in the main.c file.

0690X00000D8vfEQAR.png

Then, in Cortex-M7 project you can find the connection from A7 processor to the Virtual UART created before from M4 processor:

0690X00000D8vfYQAR.png

The full application aims to build a user interface on the LCD touch screen via GtkBuilder on Cortex-A7.

Then you'll obtain three graphic buttons that, once pressed, send a message through IPCC to the Cortex-M4.

This one receives the message, decode it and toggles the related LED:

0690X00000D8vg2QAB.png

Please note that in this project first the Cortex-M4 has to create the virtual UART and then the Cortex-A7 can connect to this UART.

Hope it could be useful.

Regards

Nicola

AShva.1
AShva.1Author
Associate III
Feb 10, 2020 6:36 AM UTC

Nicola!

thank you very much!!!

I will do and write...

Best regards

Alexander.

AShva.1
AShva.1Author
Associate III
Feb 11, 2020 11:31 AM UTC

Nicola!

I'm trying import project cortex_M4-hrdbtn_IPCC to System Workbech for STM32 IDE.

Very much errors :(

Please, write me, how to do it right.

Best regards

Alexander.

operating system: Ubuntu 16.04

nick67
Associate
Feb 11, 2020 2:54 PM UTC

Hi Alexander,

my fault. I didn't remember to mention that the projects are for STM32CubeIDE 1.2.0

You can download it from this page:

https://www.st.com/en/development-tools/stm32cubeide.html

Best regards

Nicola

operating system : XUbuntu 18.04

AShva.1
AShva.1Author
Associate III
Feb 12, 2020 6:36 AM UTC

Hi Nicola!

Thank you!

I will try. :)

Best regards

Alexander.

AShva.1
AShva.1Author
Associate III
Feb 12, 2020 11:50 AM UTC

Hi, Nicola!

Many thanks.

Your project works great. :)

I have a few new questions:

  1. How to organize a transmission channel from M4 to A7?
  2. Can i use OPENAMP without HAL?

I would be very happy if you provide examples. :)

Best regards

Alexander.

nick67
Associate
Feb 12, 2020 4:42 PM UTC

Hi, Alexander.

I'm glad to hear that the project works for you.

Unfortunately I didn't develop any more this kind of application so I can't provide other examples about IPCC :worried_face:

My first attempts started with the project OpenAMP_TTY_echo (attached here for your convenience) from STM32Cube_FW_MP1_V1.1.0 : https://wiki.st.com/stm32mpu/wiki/Install_STM32Cube_MP1_package

Lately I'm trying to have a better understanding of ADC management, peripheral sharing between CA7 and CM4 and Device Tree usage in OpenSTLinux.

Best regards

Nicola

AShva.1
AShva.1Author
Associate III
Feb 13, 2020 6:21 AM UTC

Hi, Nicola!

I understood you.

Many thanks for the help.

Best regards

Alexander.