Solved
STM32L433 LL SPI sending too much data (16 instead 8)
Hello. I need ability to send only 8 bit at the time. And I can't figure-out why I can send it, it keeps generating 16clocks no matter what
LL_GPIO_ResetOutputPin(GPIOA,LL_GPIO_PIN_4);
Delay(0x8);
while((SPI1->SR&SPI_SR_TXE)!=SPI_SR_TXE);
SPI1->DR = i;
while((SPI1->SR&SPI_SR_RXNE)!=SPI_SR_RXNE);
b = SPI1->DR;
i++;
Delay(0x2F);
LL_GPIO_SetOutputPin(GPIOA,LL_GPIO_PIN_4);By reading reference manual i know it has something to do with FIFO, but i can't chane anything for only 8bit communication
Any simple solution ?
SPI INIT code:
static void MX_SPI1_Init(void)
{
LL_SPI_InitTypeDef SPI_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SPI1);
LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOA);
/** PA4 ------> SPI1_CS#
PA5 ------> SPI1_SCK
PA6 ------> SPI1_MISO
PA7 ------> SPI1_MOSI */
GPIO_InitStruct.Pin = LL_GPIO_PIN_5|LL_GPIO_PIN_6|LL_GPIO_PIN_7;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_5;
LL_GPIO_Init(GPIOA, &GPIO_InitStruct);
SPI_InitStruct.TransferDirection = LL_SPI_FULL_DUPLEX;
SPI_InitStruct.Mode = LL_SPI_MODE_MASTER;
SPI_InitStruct.DataWidth = LL_SPI_DATAWIDTH_8BIT;
SPI_InitStruct.ClockPolarity = LL_SPI_POLARITY_LOW;
SPI_InitStruct.ClockPhase = LL_SPI_PHASE_1EDGE;
SPI_InitStruct.NSS = LL_SPI_NSS_SOFT;
SPI_InitStruct.BaudRate = LL_SPI_BAUDRATEPRESCALER_DIV64;
SPI_InitStruct.BitOrder = LL_SPI_MSB_FIRST;
SPI_InitStruct.CRCCalculation = LL_SPI_CRCCALCULATION_DISABLE;
SPI_InitStruct.CRCPoly = 7;
LL_SPI_Init(SPI1, &SPI_InitStruct);
//SPI1->CR2 |= SPI_CR2_FRXTH; try that, does not efect anything
LL_SPI_SetStandard(SPI1, LL_SPI_PROTOCOL_MOTOROLA);
LL_SPI_EnableNSSPulseMgt(SPI1);
LL_SPI_Enable(SPI1);
}