Skip to main content
NGugg.1
Associate
February 7, 2020
Question

STM32L072 (B-L072Z-LRWAN1) - SPI2 not working

  • February 7, 2020
  • 4 replies
  • 935 views

Hi,

I'm working with B-L072Z-LRWAN1 platform and struggle to see a signal on SPI2.

My SPI2 is connected on an accelerometer. It is configured as follow:

void HW_IMU_SPI_Init( void )
{
 /*##-1- Configure the SPI peripheral */
 /* Set the SPI parameters */
 
 hspi2.Instance = SPI2;
 hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
 hspi2.Init.Direction = SPI_DIRECTION_2LINES;
 hspi2.Init.Mode = SPI_MODE_MASTER;
 hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi2.Init.CLKPhase = SPI_PHASE_1EDGE;
 hspi2.Init.DataSize = SPI_DATASIZE_8BIT;
 hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; 
 hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi2.Init.NSS = SPI_NSS_SOFT;
 hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
 
 IMU_SPI_CLK_ENABLE(); 
 
 if(HAL_SPI_Init( &hspi2) != HAL_OK)
 {
 /* Initialization Error */
 Error_Handler();
 }
 
 /*##-2- Configure the SPI GPIOs */
 HW_IMU_SPI_IoInit( );
}
 
void HW_IMU_SPI_IoInit( void )
{
 GPIO_InitTypeDef initStruct={0};
 
	IMU_GPIO_CLK_ENABLE();
 
 initStruct.Pin = IMU_SCLK_PIN | IMU_MISO_PIN | IMU_MOSI_PIN;
 initStruct.Mode =GPIO_MODE_AF_PP;
 initStruct.Pull =GPIO_NOPULL ;
 initStruct.Speed = GPIO_SPEED_HIGH;
 initStruct.Alternate= IMU_SPI2_AF ;
 
 HAL_GPIO_Init(GPIOB, &initStruct);
 
 initStruct.Mode = GPIO_MODE_OUTPUT_PP;
 initStruct.Pull = GPIO_NOPULL;
 
 HW_GPIO_Init( IMU_NSS_PORT, IMU_NSS_PIN, &initStruct );
 
 HW_GPIO_Write ( IMU_NSS_PORT, IMU_NSS_PIN, 1 );
}

Systemclock is configured as follow:

void SystemClock_Config(void)
{
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 
 /* Enable HSE Oscillator and Activate PLL with HSE as source */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSEState = RCC_HSE_OFF;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLMUL = RCC_PLLMUL_6;
 RCC_OscInitStruct.PLL.PLLDIV = RCC_PLLDIV_3;
 
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 
 /* Set Voltage scale1 as MCU will run at 32MHz */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
 
 /* Poll VOSF bit of in PWR_CSR. Wait until it is reset to 0 */
 while (__HAL_PWR_GET_FLAG(PWR_FLAG_VOS) != RESET) {};
 
 /* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2
 clocks dividers */
 RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }
}

Chip select is defined as GPIO. I can see it toggling.

I'm not quite sure what I'm missing here. Could anyone help?

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
February 7, 2020

What pins? Double check AF settings.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
NGugg.1
NGugg.1Author
Associate
February 7, 2020

It is set as Alternate Function AF0 Push-Pull.

MOSI = PB15

MISO = PB14

SCK = PB13

And I set them to very high speed.

Tesla DeLorean
Guru
February 8, 2020

Check the solder bridges, especially those relating to PB13 SB2/D13 and SB9/D3

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..