cancel
Showing results for 
Search instead for 
Did you mean: 

Read actual voltages from STPMIC1

Mark81
Associate III

I'm reading the datasheet of STMPiC1 and I wonder if there's a way to read the actual voltages and/or currents. Not the setpoint ( = control registers) but the real voltages at one moment.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PatrickF
ST Employee

Hello,

no, STPMIC1 does not offer any voltage nor current measurement capabilities.

You can measure voltages/current using external component (e.g. external delta sigma V and I ADC connected to DFSDM of STM32MP15x, which is how it could be done for motor control) or voltage using STM32MP15x ADC (be careful to keep VIN in the required ranges).

Note that STM32MP15x already have internal ADC channels connected to VDDCORE and internal VrefInt (which could be indirectly used to measure VREF+ which is usually connected to VDDA or even VDD).

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NEW ! Sidekick STM32 AI agent, see here