Skip to main content
Shubham Shivarkar
Associate II
February 1, 2020
Solved

Can I cover Vl53l0X sensor with any type of cover for protection from environment?

  • February 1, 2020
  • 1 reply
  • 1060 views

Using this sensor in medical application due to which I can't install this sensor in open and therefore have to cover it with some material which will not harm its sensitivity and sensor will also be protected.

Thank you for helping.

This topic has been closed for replies.
Best answer by John E KVAM

Yes, you can. Glass, acrylic, PMMA and polycarbonate are good choices. Most plastics are transparent to 940nm light so this list is not exhaustive.

The trick is that even the best materials are not 100% transparent - and that leads to crosstalk.

Not to worry, though. Read the section on crosstalk correction and you can see how to compensate for it.

1 reply

John E KVAM
John E KVAMBest answer
ST Employee
August 19, 2021

Yes, you can. Glass, acrylic, PMMA and polycarbonate are good choices. Most plastics are transparent to 940nm light so this list is not exhaustive.

The trick is that even the best materials are not 100% transparent - and that leads to crosstalk.

Not to worry, though. Read the section on crosstalk correction and you can see how to compensate for it.

If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.