Skip to main content
Lmali.1
Associate III
Jan 30, 2020 11:46 AM UTC
Question

Migration from Nucleo to my own board - doesn't work

Hello,

I have the Nucelo-WB55 and my own board with STM32WB55CG.

I've developed a BLE software on the Nucleo-WB55 and it works fine.

When I uploaded the software to my own board it seems to have some problems.

I configured all clocks, GPIOs and etc. (Believe I did it write).

I see the BLE device (my own board) on the list of BLEs device, but when I want to connect to the device, the device unable to connect.

When I work with Nucleo-WB55, it works fine and I can connect and see all device services.

I working with IAR IDE, and useing BLE scanner App to get the BLE devices.

What am I missing? what is the different between the MCUs and what configuration I missed??

Thanks,

Lior Malik

This topic has been closed for replies.

9 replies

Jan 30, 2020 12:09 PM UTC

Hi!

check a systick is 32MGz.

I had the same thing until I broke that 1 processor should work at the same frequency as the second one.

Regards,

Vyacheslav.

Lmali.1
Lmali.1Author
Associate III
Jan 30, 2020 1:27 PM UTC

Thanks for your comment.

I verify the SysTick and it seems to look alike.

However, I get SysTick->LOAD = 4000 - 1.

With this value the Nuecloe-WB55 works fine.

maybe am I looking on a wrong variable?

Thanks,

Lior Malik

Jan 30, 2020 1:38 PM UTC

May be could be better done using a clock configuration in CubeMX ?

I use this configuration

0690X00000Bx1mwQAB.png

Remi QUINTIN
ST Technical Moderator
Jan 30, 2020 12:30 PM UTC

​Check also the pin assignment as the chip on the Nucleo board is a 68-pin package while yours  is a 48-pin package.

Lmali.1
Lmali.1Author
Associate III
Jan 30, 2020 1:22 PM UTC

Yes, I changed the target->device to ST STM32WB55CG.

This is not the issue...

Thank you.

Lmali.1
Lmali.1Author
Associate III
Feb 5, 2020 9:30 AM UTC

I found the problem.

Because I work with internal oscillator for the BLE, the define CFG_BLE_LSE_SOURCE must be set to 1 for internal source.

Thank you all!

XPonc.1
Associate II
Aug 6, 2020 8:48 AM UTC

Hey @Lmali.1​ ,

I am facing a similar problem: advertising works but I can't connect. I also have a custom board and no external oscillator; however, setting FG_BLE_LSE_SOURCE to 1 doe not change anything.

I saw on the errata ES0394:

"2.2.1 LSI2 not usable as RF low-power clock

Description

The calibration mechanism and jitter peaks cause the LSI2 clock to exceed the maximum 500 ppm frequency

deviation specified in the Bluetooth® Low Energy standard for low-speed clock.

Workaround

Clock the Bluetooth® peripheral using the LSE oscillator, instead of the LSI2."

Do you confirm that you got it to work with LSI clock? And if yes, how?

Regards

Lmali.1
Lmali.1Author
Associate III
Aug 6, 2020 9:27 AM UTC

hey @XP.1oncet​ 

I dont really remember but, if I recall, when I set the CFG_BLE_LSE_SOURCE  to 1, everything start to work properly.

I dont think that oscillator relates to advertise/connection, so maybe you should find it in other place. But I might be wrong on this one.

Good luck