Skip to main content
Alexander Novikov
Associate II
January 29, 2020
Question

Is there any plans for MCU that has STM32F407 specs, but has CAN-FD interfaces instead of CAN?

  • January 29, 2020
  • 12 replies
  • 3053 views

..

This topic has been closed for replies.

12 replies

Tesla DeLorean
Guru
January 29, 2020

I doubt this design is going to be revisited. Talk to local sales staff/engineers.

Review new parts for commonality of foot-print, 144-pin devices have generally had the best migration path.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Uwe Bonnes
Chief
January 29, 2020

STM32G474 has no ethernet but CANFD. Did you look at the new STM32H7 variant?

Alexander Novikov
Associate II
January 29, 2020

Yes, but, STM32H7 is too overloaded with features I dont need.

Alexander Novikov
Associate II
January 29, 2020

Generally I need Cortex-M4, >120Mhz, USB FS, CAN-FD (at least 2), and Ethernet MAC. STM32F407 is closest. I see all new MCUs (G0/G4/L5 lines) now utilize CAN-FD instead of old CAN, but have no Ethernet. So I expect some new chip like STM32F407 with CAN-FD. Microchip already has SAME54 - this one is exacly what I am looking for. But SAME54 has lots of drawbacks on overall design of the other chip peripherals (DMA, clocks, timers, ADC etc...)

TDK
January 30, 2020

So the STM32H7 has everything you need but you don't want to use it because it's "overloaded with features"? How is that a problem? Why not use what you want and leave the other features untouched?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Alexander Novikov
Associate II
January 30, 2020

The problem is its price

TDK
January 30, 2020

On Digikey (qty 1):

STM32F407 is $9.29

STM32H745 is $11.71

I doubt they're going to introduce a new line of chips between those two price points.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Alexander Novikov
Associate II
January 30, 2020

On our local distributor

STM32F407ZGT6 is about 5$

STM32H745 11$

Danish1
Lead III
January 30, 2020

Given the cost of all the other bits in a project (including the major one of time and effort writing and debugging the code), that sort of price-difference is negligible for small production runs (say 10 units).

And for larger production runs I'm sure you'll be able to get a better price. I've even known cases where the the price difference reverses in sufficient quantity.

Having said that, I've been trying to port some code from stm32f7 to stm32h7 for a long time and I'm still hitting differences.

Regards,

Danish

Alexander Novikov
Associate II
January 30, 2020

I am porting from STM32F107, this is why STM32F407 is preferable - it has a lots of compatible stuff.

waclawek.jan
Super User
January 31, 2020

Porting nontrivial codebase from 'F1 all the way through 'H7 is IMO a hard and bumpy road with potentially major debugging ahead. It of course depends on the nature of the code, the ratio between "true controller" and "general purpose" code.

Now, we are not insiders here, but as others pointed out, it's unlikely ST will add a Cortex-M4 with both ETH/LCD and "controller" stuff like CAN is. The 'F4 came around when the Cortex-M7 was not ready yet. Note that their newest addition, 'G4, used up the "4" number, and is straighforwardly targeted at the 'F3 area of applications (i.e. motor). ETH goes together with LCD more into the "general computing" and "needs more horsepower" area, that's why they pair up better with the Cortex-M7.

So, in short, I wouldn't hold my breath. If you don't want to go the bumpy road, you may try the multi-chip way (either external CAN controller, or cooperating MCUs, one with CAN other with ETH) - although that's not obstacle-less and not price-optimal either, I know.

JW