Skip to main content
LZhu.1
Visitor II
January 29, 2020
Solved

Does MC_SDK require the use of coprocessor?

  • January 29, 2020
  • 1 reply
  • 796 views

We are developing an application to drive dual PMSM motors with STM32H745 and FOC algorithms and resolver sensor. The inner current loops are executed at 10 kHz, PWM carrier frequency is set to 20 kHz. Is it feasible o run the entire application code on M7 only with 30% throughput margin? Does MC_SDK require the use of M4 coprocessor?

This topic has been closed for replies.
Best answer by Claire O.

Hello LZhu.1,

So far inside the MCSDK5.4.3, for the stm32H7, we have only a M4 version available as code example. we plan to increase the stm32 coverage (also allowing user to configure his application through the MC workbench). This new version should be available for mid- 2020.

Thanks and best regards,

Claire

1 reply

Claire O.
Claire O.Best answer
ST Employee
January 30, 2020

Hello LZhu.1,

So far inside the MCSDK5.4.3, for the stm32H7, we have only a M4 version available as code example. we plan to increase the stm32 coverage (also allowing user to configure his application through the MC workbench). This new version should be available for mid- 2020.

Thanks and best regards,

Claire