Skip to main content
RBaum.1
Associate
January 29, 2020
Question

STM32f30x: How to connect PB8 and PB9 to Timer16CH1 and Timer17CH1

  • January 29, 2020
  • 3 replies
  • 775 views

Hello all,

i have a Problem on a STM32F30x as described in the question.

I can´t achieve to connect TIM16CH1 and TIM17CH1 to GPIOB 8 and 9. The goal is to get a PWM signal on these pins based on a compare match.

Both Timers are running. If i read the corresponding TIM16->CNT rest. TIM17->CNT register i can see both are counting up and restarting after a overflow occurred. But i´m not getting a signal on the pin PB8 and PB9.

Here is my code:

/**
* System clock is initalized 
*/
 
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM16, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM17, ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);
 
GPIO_PinAFConfig(GPIOB, GPIO_PinSource8, GPIO_AF_1);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource9, GPIO_AF_1);
 
GPIO_InitTypeDef GPIOB_pwm_init;
GPIOB_pwm_init.GPIO_Mode = GPIO_Mode_AF;
GPIOB_pwm_init.GPIO_OType = GPIO_OType_PP;
GPIOB_pwm_init.GPIO_Pin = (GPIO_Pin_8 | GPIO_Pin_9);
GPIOB_pwm_init.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIOB_pwm_init.GPIO_Speed = GPIO_Speed_Level_3;
GPIO_Init(GPIOB, &GPIOB_pwm_init);
 
 TIM_DeInit(TIM16);
 TIM16->CR1 |= (0x01 << 7);
 TIM16->CCMR1 |= (0x04 << 4 ) | (0x01 << 3);
 TIM16->CCER |= (0x01);
 TIM16->PSC = 71; 
 TIM16->ARR = 4000;
 TIM16->CCR1 = 2000;
 TIM_Cmd(TIM16, ENABLE); 
 
 TIM_DeInit(TIM17);
 TIM17->CR1 |= (0x01 << 7);
 TIM17->CCMR1 |= (0x04 << 4 ) | (0x01 << 3);
 TIM17->CCER |= (0x01);
 TIM17->PSC = 71; 
 TIM17->ARR = 4000;
 TIM17->CCR1 = 2000;
 TIM_Cmd(TIM17, ENABLE); 

I have spend hours reading through the reference manual but no hints.

Help is welcome!

This topic has been closed for replies.

3 replies

berendi
Principal
January 29, 2020

TIM16 and TIM17 have break functionality, where there is an additional Master Output Enable bit that must be set to get any output on the pins.

TIM16->BDTR |= TIM_BDTR_MOE;
TIM17->BDTR |= TIM_BDTR_MOE;

Tesla DeLorean
Guru
January 29, 2020

Also note that both PSC and ARR are programmed with N-1 for N states, ie 0 .. N-1

You perhaps want 0 .. 3999, with the center at 2000, ie 0..1999, 2000..3999

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
RBaum.1
RBaum.1Author
Associate
January 29, 2020

Thank you @berendi for the explanation and @clive1 for your hint.

I was able to solve the problem end the oscilloscope is showing a nice pwm signal now.

Thanks 8) :)