Skip to main content
otcagon
Associate II
January 28, 2020
Solved

I want to confirm that the BLDC motor pole number information for ST MC WB . Is the pole number for rotor or stator? I think that the pole pair number is for rotor(number of magnetic / 2). Thank you

  • January 28, 2020
  • 1 reply
  • 1285 views

..

This topic has been closed for replies.
Best answer by LucasC

Dear otcagon,

In order to optimize the motor, the pole pair number (p) at the stator must be equal to p at the rotor.

In order to find p, you have two techniques:

1) Apply a small DC current between two phases and count the number of stable positions in a rotor revolution. This number equals p.

2) p = (number of magnets)/2

Best regards,

Lucas

1 reply

LucasC
LucasCBest answer
Visitor II
February 10, 2020

Dear otcagon,

In order to optimize the motor, the pole pair number (p) at the stator must be equal to p at the rotor.

In order to find p, you have two techniques:

1) Apply a small DC current between two phases and count the number of stable positions in a rotor revolution. This number equals p.

2) p = (number of magnets)/2

Best regards,

Lucas