Skip to main content
GunkutA
Associate III
January 28, 2020
Solved

Touch GFX additional software window is empty

  • January 28, 2020
  • 12 replies
  • 2335 views

Hello I am trying to use Touch GFX. In CubeMX I installed the related software pack:

0690X00000Bwig6QAB.png

When I open the additional software part there is no option I can enable Touch GFX, it is simply empty:0690X00000Bwig1QAB.png

How can I enable it from CubeMX? Thank you beforehand.

This topic has been closed for replies.
Best answer by Martin KJELDSEN

If you're using a dual core like H747, then no additional software is available from CubeMX - Which MCU is this?

/Martin

12 replies

Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
January 28, 2020

If you're using a dual core like H747, then no additional software is available from CubeMX - Which MCU is this?

/Martin

GunkutA
GunkutAAuthor
Associate III
January 28, 2020

Yes it is dual core: STM32H747XIHx.

Martin KJELDSEN
Principal III
January 28, 2020

Sorry, CubeMX is blocking any additional software from being used in this case :( I'm not sure when that'll change or the reason for doing so outside of the dual cores being really complex.

GunkutA
GunkutAAuthor
Associate III
January 28, 2020

Is there any way can I follow in order to use Touch GFX in dual core device without using CubeMX?

Martin KJELDSEN
Principal III
January 28, 2020

Not at the moment, but we have H747 disco and eval application templates ready through the touchgfx designer if you want to try that, but you cannot use the TouchGFX Generator with it unfortunately :(

I'll try to update on the status from CubeMX on allowing additional software for dual cores.

GunkutA
GunkutAAuthor
Associate III
January 28, 2020

Thank you Martin :) appreciate it.

PKopa.1
Visitor II
April 17, 2020

@Martin KJELDSEN​  Is there any update on it? It has been 3 months now, I know we are all struggling right now and such but are there any hopes it would finally work for H747 disco?

BR Pawel

Martin KJELDSEN
Principal III
April 20, 2020

I could ask around. You cannot enable additional software for H747 dual core in CubeMX - That's not in my power to change.