Question
Wakeup does not work on USB Device(ST32F407)
My hid device is numbered and receives/transmit data from/to Win10 hid driver.
The D5: Remote Wakeup descriptor is set to 1
Unfortunately, I looked through the analyzer and saw that there were no changes of D+ D signals when installing the RWUSIG bit.
I execute the following code when WIN10 sleeps and does not send SOF packets
HAL_PCD_ActivateRemoteWakeup(&hpcd_USB_OTG_FS);
HAL_Delay(10);
HAL_PCD_DeActivateRemoteWakeup(&hpcd_USB_OTG_FS);
The RWUSIG bit is installed, but it does not give anything on the bus.