2020-01-27 12:47 AM
I apologize if this is a very simple question, but I can't seem to figure out how to change the color of a Circle in my TouchGFX project.
I know that for a Box, I can do something like...
box1.setColor(touchgfx::Color::getColorFrom24BitRGB(0, 0, 255));
box1.invalidate();I would like to do the equivalent but for a Circle, however there is no setColor() method.
I understand that Circles have something called a painter, which allows me to do...
circle1Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(0, 0, 255);...but I do not know how to re-draw the circle with the updated painter.
I've tried...
circle1.setPainter(circle1Painter);
const Rect rect(0, 0, circle1.getWidth(), circle1.getHeight());
circle1.drawCanvasWidget(rect);
circle1.invalidate();but this did not work.
I appreciate any advice you can provide.
Solved! Go to Solution.
2020-01-27 1:00 AM
Hi,
Firstly, please don't apologize!
Secondly, let me give you an example of how to change the color of a circle.
I added a background box and a circle widget (with a Color Painter). Generated code looks like this:
#include <gui_generated/screen1_screen/Screen1ViewBase.hpp>
#include <touchgfx/Color.hpp>
Screen1ViewBase::Screen1ViewBase()
{
touchgfx::CanvasWidgetRenderer::setupBuffer(canvasBuffer, CANVAS_BUFFER_SIZE);
box1.setPosition(0, 0, 480, 272);
box1.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
circle1.setPosition(200, 96, 80, 80);
circle1.setCenter(40, 40);
circle1.setRadius(40);
circle1.setLineWidth(0);
circle1.setArc(0, 360);
circle1Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(194, 51, 51));
circle1.setPainter(circle1Painter);
add(box1);
add(circle1);
}
void Screen1ViewBase::setupScreen()
{
}I'll then add a button and an interaction that calls a virtual function to change the color of the circle - The following code changes the color of the circle to green upon pressing my button. Since the circle owns the painter, invalidate the circle to force a re-render of the circle.
void Screen1View::changeColor()
{
circle1Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(0, 255, 0));
circle1.invalidate();
}You could also achieve this using an image painter, of course (red image), but if you're after something simple this is the way to go.
/Martin
2020-01-27 1:00 AM
Hi,
Firstly, please don't apologize!
Secondly, let me give you an example of how to change the color of a circle.
I added a background box and a circle widget (with a Color Painter). Generated code looks like this:
#include <gui_generated/screen1_screen/Screen1ViewBase.hpp>
#include <touchgfx/Color.hpp>
Screen1ViewBase::Screen1ViewBase()
{
touchgfx::CanvasWidgetRenderer::setupBuffer(canvasBuffer, CANVAS_BUFFER_SIZE);
box1.setPosition(0, 0, 480, 272);
box1.setColor(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));
circle1.setPosition(200, 96, 80, 80);
circle1.setCenter(40, 40);
circle1.setRadius(40);
circle1.setLineWidth(0);
circle1.setArc(0, 360);
circle1Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(194, 51, 51));
circle1.setPainter(circle1Painter);
add(box1);
add(circle1);
}
void Screen1ViewBase::setupScreen()
{
}I'll then add a button and an interaction that calls a virtual function to change the color of the circle - The following code changes the color of the circle to green upon pressing my button. Since the circle owns the painter, invalidate the circle to force a re-render of the circle.
void Screen1View::changeColor()
{
circle1Painter.setColor(touchgfx::Color::getColorFrom24BitRGB(0, 255, 0));
circle1.invalidate();
}You could also achieve this using an image painter, of course (red image), but if you're after something simple this is the way to go.
/Martin