Skip to main content
MEwen.1
Associate II
January 25, 2020
Question

Looking for an appraisal of the Chinese STM32H750 board advertised on Ebay, Alibaba, etc. Does ST sell any equivalent product? I'm finding this website very difficult to navigate, and I can't find one.

  • January 25, 2020
  • 7 replies
  • 2622 views

I'm sorry if I'm in the wrong forum.  The Chinese board is at https://www.ebay.co.uk/itm/STM32H750VBT6-Development-Board-ARM-STM32H7-Programmable-Controller-Module/123952880379?hash=item1cdc2adafb:g:8vsAAOSwnihdtAn4

It has a USB port on it with a CH340C on it - but I don't know if it can be programmed through the USB. It also has an SD card slot, so maybe program can be transported to it on the SD card. Apart from the picture, I don't know anything about it, and experience tells me there will be little or no documentation.

Does STM offer anything equivalent? If so, can't find it on the website.

This topic has been closed for replies.

7 replies

Piranha
Principal III
January 26, 2020

For a cheap board, just take some Nucleo board and connect necessary additional electronics when needed. Besides schematics and documentation, the main advantage is:

  • On-board ST-LINK debugger/programmer with USB re-enumeration capability: mass storage, Virtual COM port and debug port

Additionally the on-board ST-LINK can be converted to J-Link. Developing without debugger in 21st century is pure masochism...

Pavel A.
January 26, 2020

I wish I could buy a Nucleo board with H750. DISCO's are too expensive unless you need the LCD.

So I prototyped most things including Ethernet on Nucleo H743, and H75x specific things only (secure boot ...) on the chinese board.

-- pa

berendi
Principal
January 26, 2020

I don't think it can be programmed by SD card.

It might be programmable through the USB-serial port, but you'd certainly need an ST-Link or compatible adapter for debugging.

Tesla DeLorean
Guru
January 26, 2020

A loader that can pull from SD into RAM is certainly possible.

Board ships with simple LED toggle, as I recall.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
waclawek.jan
Super User
January 26, 2020

Some discussion of this (or similar) board here and here.

I'd assume the CH340 is connected so that the built-in bootloader could be used in USART mode. Maybe some of the unpopulated parts around the CH340 are the circuitry to automate reset/BOOT0 handling connecting them to DTR/RTS.

JW

Tesla DeLorean
Guru
January 26, 2020

Thanks, was trying to remember/guess the right terms for the search, unsuccessfully.

#H750VB

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
hansd56
Senior
January 26, 2020

And still Y silicon.

Pavel A.
January 26, 2020

I've bought two boards, in these the silicon is V,

Posted the Cube .ioc file here.

-- pa

Tesla DeLorean
Guru
January 26, 2020

Mine was a Y, but suspect newer stock is probably available now.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
hansd56
Senior
January 26, 2020

And it has a SWD port. So it can be programmed with an external debugger.

Tesla DeLorean
Guru
January 26, 2020
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
January 26, 2020

I have this board, programming via SWD header into an ST-LINK/V2

Have SD Card working.

SPI Flash is not wired in a QUADSPI mode

No SDRAM.

Good break-out connectivity

ST has a DISCO board. STM32H750B-DK https://www.st.com/en/evaluation-tools/stm32h750b-dk.html

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
RMcCa
Senior II
January 26, 2020

Can you layout PCBs?

Small prototype pcbs are cheap from Shenzen. I've had really good luck designing and building boards for stm32f730 and am working with h7s now.​