Skip to main content
VChur.1
Associate II
January 24, 2020
Question

my B-L475E-IOT1A2 want not to connect AWS!

  • January 24, 2020
  • 5 replies
  • 1589 views

I have tried setup into device all of kind CA certificates from AWS https://docs.aws.amazon.com/iot/latest/developerguide/server-authentication.html

followin instruction from ST but nothing help!! Only errors:

*** AWS connectivity demonstration ***

AWS IoT SDK Version 2.1.1-

MQTT connection in progress:  Attempt 1/3 ...

C:\STM32_IoT_Cloud_Workspace_V1.0.1\Middlewares\Third_Party\mbedTLS\library\ssl_tls.c:4454: x509_verify_cert() returned -9984 (-0x2700)

ERROR: iot_tls_connect L#303 failed

 ! mbedtls_ssl_handshake returned -0x2700

ERROR: iot_tls_connect L#311   Unable to verify the server's certificate. Either it is invalid,

  or you didn't set ca_file or ca_path to an appropriate value.

This topic has been closed for replies.

5 replies

AKlei.1
Visitor II
January 27, 2020

+1

I have exactly the same problem and also looking for an answer to this one.

I've created the AWS certificates and installed as per instructions and I get the same error.

(We have been able to successfully create AWS certificates for other (Non-STM32) based platforms we are using)

AKlei.1
Visitor II
January 28, 2020

@VChur.1​  ... I managed to get it working.

When you download the software from this site ... https://my.st.com/content/my_st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32cube-expansion-packages/x-cube-aws.html ...

... you have the option of "Download" ... "Get Software" or "Previous Versions" ... "1.2.1". I found that version 1.2.1 worked from me.

VChur.1
VChur.1Author
Associate II
January 31, 2020

@AKlei.1​  Thank you for this information! Please help me how to add expansion package (x-cube-aws for example) to STM32CUBE IDE ?

I cant find any information about it ... for example, if I try to add via "help/Embedded Software Packages Manager" it write me "Problem during load of selected File" - "Invalid zip file or missing expected Pdsc file within pack root directory."

And many "water" information about "Expansion Packages" and none instruction how to add it to STM32CubeIDE !!!!!!

AKlei.1
Visitor II
February 2, 2020

@VChur.1​ , Sorry I'm not using the STM32CUBE IDE