Skip to main content
GMeur
Associate III
January 24, 2020
Solved

Simulator in project upgrated to TouchGFX 4.13 won't work

  • January 24, 2020
  • 3 replies
  • 959 views

Hej Hej,

Since I upgrated my project from version 4.12 to 4.13, the simulator won't launch anymore (the project was initially created with TouchGFX 4.10). VS throws two error msgs :

1) unresolved external symbols void __cdecl touchgfx::simulator_enable_stdio(void) in the function void __cdecl touchgfx_enable_stdio(void)

2) unresolved external symbols void __cdecl touchgfx::simulator_printf(char const*, char*) in the function void __cdecl touchgfx_printf(char const*,...)

It seems it's related to a known issue but my project does use HALSDL2 and the functions mentioned in the joined article are present in the HALSDL2.cpp file so the problem stems from somewhere else.

How can I solve it?

I'm sure it's trivial but any guidance would be more than welcomed.

Thanks in advance.

This topic has been closed for replies.
Best answer by jimmii

Had the same problem...

The $(TouchGFXEnvPath) Macro Variable was not updated to the latest installation path.

After updating these, it worked...

0690X00000BwVk0QAF.png

3 replies

Martin KJELDSEN
Principal III
January 24, 2020

I think you'll have to send me your project. Can you do that?

/Martin

jimmii
jimmiiBest answer
Senior II
January 24, 2020

Had the same problem...

The $(TouchGFXEnvPath) Macro Variable was not updated to the latest installation path.

After updating these, it worked...

0690X00000BwVk0QAF.png

GMeur
GMeurAuthor
Associate III
January 27, 2020

Thanks Jimmii!