Skip to main content
Martin KJELDSEN
Principal III
Jan 23, 2020 12:59 PM UTC
Question

FIX: STM32F746G-DISCO V3.0 TouchGFX Application Template (CubeIDE)

Hi everyone,

Just a heads up regarding the new (v3.0) STM32F746G-DISCO application template. As some of you have experienced, when using CubeIDE, the project was referencing some non-existant files and the Post-Generate command (after pressing Generate Code in TouchGFX designer) was not able to clean these up, which it can for other IDE/project types.

When compiling some of you saw this error:

make: *** No rule to make target 'C:/TouchGFXProjects/YetAnotherTest/TouchGFX/gui/src/logoargbbilinear127qspi_screen/LogoARGBBilinear127QSPIPresenter.cpp', needed by 'Application/User/gui/LogoARGBBilinear127QSPIPresenter.o'. Stop.

I've fixed and uploaded the Application Template so you no longer have this issue. To fix it manually you can:

  • Delete the file references from the .project file
  • Re-generate the project from CubeMX and then Generate Code from TouchGFX designer.

But, as said, going forward any project hat is based on STM32F746G-DISCO from the designer does not have these issues.

Sorry for the inconvenience, and thanks for reporting the issue.

/Martin

This topic has been closed for replies.

20 replies

tushar_tp
Associate III
Jan 23, 2020 7:15 PM UTC

Hello Martin,

I have installed TouchGFX 4.13 and I am not able to see the V3.0 templates in the online applications.

Where can I see the V3.0 templates?

Thanks,

Tushar

0690X00000BwUK1QAN.jpg

tushar_tp
Associate III
Jan 23, 2020 7:26 PM UTC

Sorry Martin, I forget to change the board from Simulator to specific boards. After Changing to Specific boards I am able to see v3.0.0 templates

Martin KJELDSEN
Principal III
Jan 23, 2020 9:03 PM UTC

That's quite allright :) Glad you figured it out @tushar_tp​ 

/Martin

chaaalyy
Senior II
Mar 4, 2020 8:56 PM UTC

Strange... I built a template for CubeIDE 1.3.0, based on the blank ui. When it comes to choose another template in designer (file -> new), on the left i can choose "application template" STM32F746Discovery Kit in V3.0.0 but on the right side all the ui templates are 1.0.0, 1.1.0 or 2.0.0... Absolutely nothing in V3. Also in "online applications" i see just one app for the H750B-board and two washerdemos in V1.0.0 (as in the picture above). Of course i changed from simulator to my f746-board V3, but the shown apps and templates never change ...

/Charly

Asantos
Associate III
Jan 23, 2020 11:50 PM UTC

Martin, thank you very much.

Now I can generate a touchGFX designer project using the F746-DISCO template that compiles for the STM32CubeIDE and for the EWARM. 

The RadioButton UI example don´t generate external QSPI code, so using this one, I can flash the board using the STM32CubeIDE and the EWARM.

If I use the ProgressIndicator UI example, that generate external QSPI code, I only can flash the board using the EWARM. 

For while it is not a problem to me because we use EWARM as IDE.

My challenge now is how to install the F746-DISCO template offline. Comparing the directory .../TouchGFX/4.13.0 of a computer without the template with the same directory of a computer with the template installed, I couldn't note difference.

egoltzman
Senior
Jan 28, 2020 9:04 AM UTC

I was able to build a project successfully with the F746 AT but when I try to debug it I get this:

Download verified successfully 
(Read)Failed determine breakpoint type
Error! Failed to read target status 
Debugger connection lost.
Shutting down...
 

I saw that it was happen to others, I did not found a solution here, did I missed it?

Martin KJELDSEN
Principal III
Jan 28, 2020 9:51 AM UTC

Having the same issue - Trying to investigate a bit.

egoltzman
Senior
Jan 28, 2020 11:50 AM UTC

Yes, I have also had this, and since the F746 did not worked I moved to the F69 that is working under the debugger

Francois1
Visitor II
Feb 14, 2020 6:38 PM UTC

@Martin KJELDSEN​ 

Same problem with F746G-DISCO no solution

(Read)Failed determine breakpoint type

Error! Failed to read target status

Debugger connection lost.

any news ???

dave239955_st
Visitor II
Mar 27, 2020 11:32 PM UTC

Exactly the same problem here. Seems CubeIDE isnt really ready for prime time :\

Martin KJELDSEN
Principal III
Apr 1, 2020 10:40 AM UTC

I have a fix for this CubeIDE debugger issue. I just forgot to upload a new template - Will get on it ASAP!

DSchm.3
Associate
Apr 23, 2020 10:50 AM UTC

Hello Martin, have you already uploaded the new template?

Martin KJELDSEN
Principal III
Apr 23, 2020 12:30 PM UTC

Yeah it's up. Look for version 3.0.1