STM32 CubeMX & STM32 Cube ide integration with Touch GFX
Hello I have STM32H747I_DISCO board. I can use and program the MCU in it from the STM32Cube ide (such as LED Blinking etc.). Also I can show some simple things on the display on it by using Touch GFX Designer application. But when I program the MCU after that when I insert Touch GFX output into the board, led blinking disappers and I can only use display. So I need a way to use Touch GFX in STM32Cube ide. Is there a way to do it? In CubeMX there is no Graphics option in Middlewares. I believe that is where you enable the Touch GFX. How can I enable and use it? Thanks beforehand.