Skip to main content
J.Yun
Associate
January 20, 2020
Question

STM32L432KC HSE (external clock source) without using MCO from ST-Link

  • January 20, 2020
  • 9 replies
  • 2492 views

Hello,

​

I would like to ask you one question.

In the datasheet of NUCLEO-L432KC, MCO output from ST-Link MCU should be used for input clock of L432KC MCU to use/enable HSE option.

I wonder if I can use HSE without using MCO output from ST-LINK MCU.

I want to connect external XTAL for HSE option, but there is only clock_input pin on L432KC (there's no clock_output pin for HSE).

Thank you in advance for your reply.

This topic has been closed for replies.

9 replies

berendi
Principal
January 20, 2020

If it's not in the datasheet, then it's not possible. What do you need it for?

J.Yun
J.YunAuthor
Associate
January 20, 2020

Just curiosity.

In the datasheet, I can get a more precise frequency if I use 8 MHz XTAL (MCO from ST-LINK).

I am working on frequency-related project, so I just want to improve the freq. accuracy.

If it is impossible, I have no choice but to change the MCU to G431KB that uses HSE clock.

J.Yun
J.YunAuthor
Associate
January 20, 2020

Or I can add additional circuit for HSE in my customized PCB layout.

  1. 8MHz XTAL driving circuit.
  2. Readout circuit (its output will replace the MCO output from ST-LINK MCU).
waclawek.jan
Super User
January 20, 2020

You can't use a crystal, but you can connect a crystal oscillator such as https://global.kyocera.com/prdct/electro/product/crystal-device/clock/ or similar from any other manufacturer.

You'd need to disconnect MCO from CK_IN, of course.

JW

J.Yun
J.YunAuthor
Associate
January 20, 2020

I would appreciate if you could explain the difference between XTAL and crystal oscillator you mentioned.

I think they are same, Isn't it?

waclawek.jan
Super User
January 20, 2020

The terminology is confusing, I know.

Crystal as a part is a passive two-terminal device (even if it is packaged in four-pin package, especially SMD crystals are). They need to be connected into a circuit, and this circuit (and this is the confusion) is then called crystal oscillator.

Crystal oscillator as a part is an active device with at least three pins - ground, power supply and output - usually packaged in four pin package, whether it's through-hole or SMD, and it generates a digital-level signal of a specified frequency without any other external circuitry. Sometimes the fourth pin is active and acts as an enable/output gate. Sometimes these are marked as XO or SXO (for Simple Crystal Oscillator); then there are derivatives of these with added value, such as VCXO (Voltage Controlled XO) or TCXO (Temperature Compensated XO).

JW

J.Yun
J.YunAuthor
Associate
January 20, 2020

Really helpful comment! ​

I will go over them!

Have a good day :D