Skip to main content
AStaa.1
Associate
January 17, 2020
Question

STM32G4 ADC running in low speed

  • January 17, 2020
  • 7 replies
  • 1601 views

The new STM32G474RE has an ADC that can run up to 4MSPS.

I'm doing a project where I need to do the sampling in 1MSPS. But the maximum sample rate achieved was 300kSPS. When I set timer 1 for the ADC trigger to 500kSPS the "while" loop simply locks. Seems to be all right with ADC setup, but I can't solve this problem.

#include "main.h"
 
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;
 
TIM_HandleTypeDef htim1;
 
uint32_t leitura_ad[2];
uint32_t cont=0;
 
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_ADC1_Init(void);
static void MX_DMA_Init(void);
static void MX_HRTIM1_Init(void);
static void MX_TIM1_Init(void);
 
int main(void)
{
 HAL_Init();
 
 SystemClock_Config();
 
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_ADC1_Init();
 MX_HRTIM1_Init();
 MX_TIM1_Init();
 
 if (HAL_ADC_Start_DMA(&hadc1,
 (uint32_t *) leitura_ad, 1
 ) != HAL_OK)
 {
 Error_Handler();
 }
 
 HAL_TIM_Base_Start(&htim1);
 
 while (1)
 {
	 HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
	 HAL_Delay(100);
 }
}
 
 
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
 
 /** Configure the main internal regulator output voltage 
 */
 HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1_BOOST);
 /** Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV3;
 RCC_OscInitStruct.PLL.PLLN = 40;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_7) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the peripherals clocks 
 */
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_ADC12;
 PeriphClkInit.Adc12ClockSelection = RCC_ADC12CLKSOURCE_PLL;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 Error_Handler();
 }
}
 
/**
 * @brief ADC1 Initialization Function
 * @param None
 * @retval None
 */
static void MX_ADC1_Init(void)
{
 
 /* USER CODE BEGIN ADC1_Init 0 */
 
 /* USER CODE END ADC1_Init 0 */
 
 ADC_MultiModeTypeDef multimode = {0};
 ADC_ChannelConfTypeDef sConfig = {0};
 
 /* USER CODE BEGIN ADC1_Init 1 */
 
 /* USER CODE END ADC1_Init 1 */
 /** Common config 
 */
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV2;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.GainCompensation = 0;
 hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 hadc1.Init.LowPowerAutoWait = DISABLE;
 hadc1.Init.ContinuousConvMode = DISABLE;
 hadc1.Init.NbrOfConversion = 1;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConv = ADC_EXTERNALTRIG_T1_TRGO;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_RISING;
 hadc1.Init.DMAContinuousRequests = ENABLE;
 hadc1.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
 hadc1.Init.OversamplingMode = DISABLE;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure the ADC multi-mode 
 */
 multimode.Mode = ADC_MODE_INDEPENDENT;
 if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
 {
 Error_Handler();
 }
 /** Configure Regular Channel 
 */
 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = ADC_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
 sConfig.SingleDiff = ADC_SINGLE_ENDED;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC1_Init 2 */
 
 /* USER CODE END ADC1_Init 2 */
 
}
 
static void MX_TIM1_Init(void)
{
 
 /* USER CODE BEGIN TIM1_Init 0 */
 
 /* USER CODE END TIM1_Init 0 */
 
 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};
 TIM_BreakDeadTimeConfigTypeDef sBreakDeadTimeConfig = {0};
 
 /* USER CODE BEGIN TIM1_Init 1 */
 
 /* USER CODE END TIM1_Init 1 */
 htim1.Instance = TIM1;
 htim1.Init.Prescaler = 0;
 htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim1.Init.Period = 640;
 htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim1.Init.RepetitionCounter = 0;
 htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
 sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_UPDATE;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sBreakDeadTimeConfig.BreakAFMode = TIM_BREAK_AFMODE_INPUT;
 sBreakDeadTimeConfig.Break2AFMode = TIM_BREAK_AFMODE_INPUT;
 if (HAL_TIMEx_ConfigBreakDeadTime(&htim1, &sBreakDeadTimeConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM1_Init 2 */
 
 /* USER CODE END TIM1_Init 2 */
 
}
 
/** 
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void) 
{
 
 /* DMA controller clock enable */
 __HAL_RCC_DMAMUX1_CLK_ENABLE();
 __HAL_RCC_DMA1_CLK_ENABLE();
 
 /* DMA interrupt init */
 /* DMA1_Channel1_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Channel1_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Channel1_IRQn);
 
}
 
/**
 * @brief GPIO Initialization Function
 * @param None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 
 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOF_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 
 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET);
 
 /*Configure GPIO pin : PA5 */
 GPIO_InitStruct.Pin = GPIO_PIN_5;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
}
 
/* USER CODE BEGIN 4 */
 
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc1){
 
	cont++;
	//HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
 
}

This topic has been closed for replies.

7 replies

oeliks
Associate III
January 17, 2020

Sorry, wrong theead.​

Dvorak.Peter
Associate II
January 18, 2020

"I need to do the sampling in 1MSPS"

Looks like HAL needs faster processor to keep up with the ADC.

HAL is not code or speed efficient

AStaa.1
AStaa.1Author
Associate
January 20, 2020

The processor is running at 160MHz and the ADC uses reading via DMA. Do you refer to the ADC lib HAL or the other peripherals?

Even using the HAL and DMA libs, I am still a long way from 4MSPS, and that I cannot understand.

If I start reading 4 channels in 250KSPS the same code works very well, and in my understanding it is the equivalent of reading 1 channel in 1MSPS.

waclawek.jan
Super User
January 20, 2020

> if (HAL_ADC_Start_DMA(&hadc1,

> (uint32_t *) leitura_ad, 1

I don't use Cube, but doesn't this mean that the DMA ISR will be called after every single ADC conversion?

JW

Dvorak.Peter
Associate II
January 21, 2020

And the interrupt service takes longer then a single ADC conversion.

See:

Getting Started with STM32 - Working with ADC and DMA

https://www.digikey.com/en/maker/projects/getting-started-with-stm32-working-with-adc-and-dma/f5009db3a3ed4370acaf545a3370c30c

Ozone
Principal
January 21, 2020

I can't see any interrupt handler code.

Check it's runtime, including all the HAL-generated callbacks.

I don't use Cube either.

AStaa.1
AStaa.1Author
Associate
January 23, 2020

I managed to solve the problems.

HAL actually enables all possible interruptions. The solution was to disable all ADC and DMA interruptions:

...
 
 if (HAL_ADC_Start_DMA(&hadc1,(uint32_t *) leitura_ad, 1) != HAL_OK){
 Error_Handler();
 }
 
 __HAL_ADC_DISABLE_IT(&hadc1, (ADC_IT_RDY | ADC_IT_EOSMP | ADC_IT_EOC | ADC_IT_EOS | ADC_IT_OVR | ADC_IT_JEOC | ADC_IT_JEOS | ADC_IT_AWD1 | ADC_IT_AWD2 | ADC_IT_AWD3 | ADC_IT_JQOVF));
 
 __HAL_DMA_DISABLE_IT(&hdma_adc1, (DMA_IT_TC | DMA_IT_HT | DMA_IT_TE));
 
...

Later I only enabled DMA TC interrupt:

 __HAL_DMA_ENABLE_IT(&hdma_adc1, DMA_IT_TC);

This way I got 500KSPS.

Finally I changed the function to clear the interrupt flag (HAL_DMA_IRQHandler(&hdma_adc1)) to write directly to the register IFCR:

void DMA1_Channel1_IRQHandler(void)
{
	cont++;
 
 //HAL_DMA_IRQHandler(&hdma_adc1);
 
	DMA1->IFCR = 0x07;
}

With these changes I managed to reach 1MSPS.

Thanks for the help.