Skip to main content
Nawres GHARBI
ST Technical Moderator
Jan 17, 2020 9:31 AM UTC
Question

Migration issue from 5.4.0 to 5.5.0

Dear customers,

We are facing a little issue during the migration from the 5.4.0 to the 5.5.0 (reported in this thread https://community.st.com/s/question/0D50X0000BxzZV9SQM/upgraded-stm32cubemx-from-540-to-550-and-now-it-fails-to-generate-the-project)

To avoid having this problem, please migrate to the 5.5.0 by installing the new package from the web and not updating from the tool.

Best regards,

STM32CubeMX team

This topic has been closed for replies.

6 replies

Karl Yamashita
Principal
Jan 21, 2020 1:15 AM UTC

I'm using 5.5.0 and want to import a 5.4.0 project but the Import Project is grayed out. This is a fresh install

0690X00000BwFjLQAV.jpg

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Nawres GHARBI
ST Technical Moderator
Jan 22, 2020 8:19 AM UTC

Hello @Community member​ 

Import do work only on a fresh loaded MCU, importing on a configured MCU (like in the screenshot) will be available in a future release of MX

Zoey
Associate III
Feb 12, 2020 12:14 PM UTC

I firstly removed the 5.5.0 which was installed via update tools and then install 5.5.0. However, it still failed to generate the project.0690X00000D9kegQAB.png

1kvin
Visitor II
Feb 24, 2020 8:21 PM UTC

I have the same problem0690X00000DXDEEQA5.jpg

Aymen CHAKROUN
ST Employee
Feb 25, 2020 7:25 AM UTC

I guess you are using Java13. If yes, please remove this version and install at least Java11 or Java8. We found an issue with Java13/Keil IDE, this issue is not related to STM32CubeMX upgrade process.

For info: STM32CubeMX is not yet validated/tested with Java13.

Zoey
Associate III
Mar 4, 2020 1:22 PM UTC

The new 5.6.0 with Java 8 still has the same error.​