when trying to connect with the serial port this is the message I got and the uart connection is completely lost and is there any possibility to reestablish the connection?
11:17:48:304 : Serial Port COM8 is successfully opened.
11:17:48:304 : Port configuration: parity = even, baudrate = 9600, data-bit = 8, stop-bit = 1.0, flow-control = off
11:17:48:304 : No Init bits value is : 0
11:17:48:304 : Sending init command:
11:17:48:304 : byte 0x7F sent successfully to target
11:17:49:304 : Wait ends after 1 loop, dataready = 0, delay = 1000
11:17:49:305 : Timeout error occured while waiting for acknowledgement.
11:17:49:305 : No response from target received
11:17:49:306 : byte 0x7F sent successfully to target
11:17:49:404 : Wait ends after 1 loop, dataready = 0, delay = 100
11:17:49:405 : Timeout error occured while waiting for acknowledgement.
11:17:49:406 : No response from target received
11:17:49:406 : Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...