cancel
Showing results for 
Search instead for 
Did you mean: 

SWO viewer for STM32CubeProgrammer?

aonsquared
Associate III

Hi,

We're currently using the SWO viewer in the old ST-Link Utility in Windows.

However, this is a bit inconvenient for us because our main development is in Linux. Is SWO support planned for STM32CubeProgrammer? Even just STM32Programmer_CLI SWO support would be much appreciated.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Houda GHABRI
ST Employee

Hi @aonsquared​ @psztoch​ ,

I come back to the this thread to announce that SWO viewer is now supported in 2.6.0 (also in 2.5.0).

Hope this helps other users using SWO.

Houda

View solution in original post

2 REPLIES 2
psztoch
Associate II

No support for SWO is very important lack in feature list!!!

It should support use of shared st-link-server.

It should support connection via TCP port using st-link_gdbserver, too.

Houda GHABRI
ST Employee

Hi @aonsquared​ @psztoch​ ,

I come back to the this thread to announce that SWO viewer is now supported in 2.6.0 (also in 2.5.0).

Hope this helps other users using SWO.

Houda