Skip to main content
TLahr.1
Associate II
January 12, 2020
Question

Multiple Definitions Errors

I am getting compiling errors when trying to include a custom class into a TouchGFX project.

I made a class called "test" with it's test.h and test.cpp components.

//File: test.h
 
#pragma once
class test
{
public:
 test();
 ~test();
 
 void set_testX(int);
 int get_testX();
 
protected:
 int testX;
};
 
#include "test.cpp"
//File: test.cpp
 
#include "test.h"
 
test::test()
{
 testX = 0;
}
 
test::~test()
{
}
 
void test::set_testX(int x)
{
 testX = x;
}
 
int test::get_testX()
{
 return testX;
}

When I include test.h into mainScreenView.cpp (generated from TouchTFX) the code compiles fine.

However, I want test.h to be included into mainScreenView.hpp... When I attempt this, I get multiple definition erorrs, and I have no idea how to fix this....:sad_but_relieved_face:

//File: mainScreenView.cpp
//This code compiles fine when the test.h include is not commented out
 
#include <gui/mainscreen_screen/mainScreenView.hpp>
#include <gui_generated/mainscreen_screen/mainScreenViewBase.hpp>
#include "BitmapDatabase.hpp"
#include <texts/TextKeysAndLanguages.hpp>
#include <touchgfx/Color.hpp>
//#include <../../simulator/msvs/test.h> //commented out to include in the .hpp
 
using namespace std;
 
mainScreenView::mainScreenView()
{
 
}
 
void mainScreenView::setupScreen()
{
 mainScreenViewBase::setupScreen();
}
 
void mainScreenView::tearDownScreen()
{
 mainScreenViewBase::tearDownScreen();
}
 
void mainScreenView::set_test_X()
{
 int x = testx.get_testX();
 //Unicode::UnicodeChar y[10] = new UnicodeChar;
 Unicode::snprintf(textArea1_1Buffer, TEXTAREA1_1_SIZE, "hello %i", x);
 textArea1_1.setWildcard(textArea1_1Buffer);
 textArea1_1.invalidate();
}
//File: mainScreenView.hpp
//This code runs into Mulitple definition errors....
 
#ifndef MAINSCREENVIEW_HPP
#define MAINSCREENVIEW_HPP
 
#include <gui_generated/mainscreen_screen/mainScreenViewBase.hpp>
#include <gui/mainscreen_screen/mainScreenPresenter.hpp>
#include <gui/introscreen_screen/introScreenPresenter.hpp>
#include <../../simulator/msvs/test.h> //trying to include test.h
 
class mainScreenView : public mainScreenViewBase
{
public:
 mainScreenView();
 virtual ~mainScreenView() {}
 virtual void setupScreen();
 virtual void tearDownScreen();
 
 virtual void set_test_X();
 virtual void setTestXValue();
protected:
 test testx;
};
 
#endif // MAINSCREENVIEW_HPP
Small section of the error:
 
Compile
 make -f ../gcc/Makefile -j8
 Converting images
 Compiling TouchGFX/gui/src/mainscreen_screen/mainScreenView.cpp
 Compiling TouchGFX/gui/src/mainscreen_screen/mainScreenPresenter.cpp
 Compiling TouchGFX/generated/gui_generated/src/common/FrontendApplicationBase.cpp
 Compiling TouchGFX/target/BoardConfiguration.cpp
 Linking TouchGFX/build/bin/target.elf
 TouchGFX/build/ST/STM32F769I-DISCO/TouchGFX/gui/src/mainscreen_screen/mainScreenPresenter.o: In function `test::test()':
 c:\TouchGFXProjects\MyApplication_7/TouchGFX/gui/include/../../simulator/msvs/test.cpp:5: multiple definition of `test::test()'
 TouchGFX/build/ST/STM32F769I-DISCO/TouchGFX/gui/src/mainscreen_screen/mainScreenView.o:c:\TouchGFXProjects\MyApplication_7/TouchGFX/gui/include/../../simulator/msvs/test.cpp:5: first defined here
 TouchGFX/build/ST/STM32F769I-DISCO/TouchGFX/gui/src/mainscreen_screen/mainScreenPresenter.o: In function `mainScreenPresenter::~mainScreenPresenter()':
 c:\TouchGFXProjects\MyApplication_7/TouchGFX/gui/include/gui/mainscreen_screen/mainScreenPresenter.hpp:28: multiple definition of `test::test()'
 TouchGFX/build/ST/STM32F769I-DISCO/TouchGFX/gui/src/mainscreen_screen/mainScreenView.o:c:\TouchGFXProjects\MyApplication_7/Middlewares/ST/TouchGFX/touchgfx/framework/include/touchgfx/Screen.hpp:213: first defined here
 TouchGFX/build/ST/STM32F769I-DISCO/TouchGFX/gui/src/mainscreen_screen/mainScreenPresenter.o: In function `mainScreenPresenter::~mainScreenPresenter()':
 c:\TouchGFXProjects\MyApplication_7/TouchGFX/gui/include/gui/mainscreen_screen/mainScreenPresenter.hpp:28: multiple definition of `test::~test()'
 TouchGFX/build/ST/STM32F769I-DISCO/TouchGFX/gui/src/mainscreen_screen/mainScreenView.o:c:\TouchGFXProjects\MyApplication_7/Middlewares/ST/TouchGFX/touchgfx/framework/include/touchgfx/Screen.hpp:213: first defined here
 TouchGFX/build/ST/STM32F769I-DISCO/TouchGFX/gui/src/mainscreen_screen/mainScreenPresenter.o: In function `mainScreenPresenter::~mainScreenPresenter()':
 c:\TouchGFXProjects\MyApplication_7/TouchGFX/gui/include/gui/mainscreen_screen/mainScreenPresenter.hpp:28: multiple definition of `test::~test()'
 TouchGFX/build/ST/STM32F769I-DISCO/TouchGFX/gui/src/mainscreen_screen/mainScreenView.o:c:\TouchGFXProjects\MyApplication_7/Middlewares/ST/TouchGFX/touchgfx/framework/include/touchgfx/Screen.hpp:213: first defined here
 TouchGFX/build/ST/STM32F769I-DISCO/TouchGFX/gui/src/mainscreen_screen/mainScreenPresenter.o: In function `mainScreenPresenter::~mainScreenPresenter()':
 c:\TouchGFXProjects\MyApplication_7/TouchGFX/gui/include/gui/mainscreen_screen/mainScreenPresenter.hpp:28: multiple definition of `test::set_testX(int)'
 TouchGFX/build/ST/STM32F769I-DISCO/TouchGFX/gui/src/mainscreen_screen/mainScreenView.o:c:\TouchGFXProjects\MyApplication_7/Middlewares/ST/TouchGFX/touchgfx/framework/include/touchgfx/Screen.hpp:213: first defined here
 TouchGFX/build/ST/STM32F769I-DISCO/TouchGFX/gui/src/mainscreen_screen/mainScreenPresenter.o: In function `mainScreenPresenter::~mainScreenPresenter()':
 c:\TouchGFXProjects\MyApplication_7/TouchGFX/gui/include/gui/mainscreen_screen/mainScreenPresenter.hpp:28: multiple definition of `test::get_testX()'

Any advice?

Thanks.

This topic has been closed for replies.

5 replies

Martin KJELDSEN
Principal III
January 13, 2020

You're including test.cpp from your headerfile where test is declared. Remove that.

#include "test.cpp"

/Martin

TLahr.1
TLahr.1Author
Associate II
January 13, 2020

Right. I tried removing that line and it gives me 'Undefined Reference' errors.

It seems I am not properly defining the class functions....?

Compile
 make -f ../gcc/Makefile -j8
 Converting images
 Compiling TouchGFX/gui/src/mainscreen_screen/mainScreenView.cpp
 Compiling TouchGFX/gui/src/mainscreen_screen/mainScreenPresenter.cpp
 Compiling TouchGFX/generated/gui_generated/src/common/FrontendApplicationBase.cpp
 Compiling TouchGFX/target/BoardConfiguration.cpp
 Linking TouchGFX/build/bin/target.elf
 TouchGFX/build/ST/STM32F769I-DISCO/TouchGFX/gui/src/mainscreen_screen/mainScreenView.o: In function `mainScreenView::set_test_X()':
 c:\TouchGFXProjects\MyApplication_7/TouchGFX/gui/src/mainscreen_screen/mainScreenView.cpp:27: undefined reference to `test::get_testX()'
 TouchGFX/build/ST/STM32F769I-DISCO/TouchGFX/gui/src/mainscreen_screen/mainScreenView.o: In function `mainScreenView::~mainScreenView()':
 c:\TouchGFXProjects\MyApplication_7/TouchGFX/gui/include/gui/mainscreen_screen/mainScreenView.hpp:13: undefined reference to `test::~test()'
 TouchGFX/build/ST/STM32F769I-DISCO/TouchGFX/gui/src/mainscreen_screen/mainScreenView.o: In function `mainScreenView::mainScreenView()':
 c:\TouchGFXProjects\MyApplication_7/TouchGFX/gui/src/mainscreen_screen/mainScreenView.cpp:10: undefined reference to `test::test()'
 collect2.exe: error: ld returned 1 exit status
 gcc/Makefile:330: recipe for target 'TouchGFX/build/bin/target.elf' failed
 make[2]: *** [TouchGFX/build/bin/target.elf] Error 1
 gcc/Makefile:326: recipe for target 'generate_assets' failed
 make[1]: *** [generate_assets] Error 2
 ../gcc/Makefile:45: recipe for target 'all' failed
 make: *** [all] Error 2
 Failed
 Failed