Skip to main content
MKhan.1
Associate
Jan 10, 2020 8:31 AM UTC
Question

STM32F042F4P6 - Input current in trigger mode.

Help find the answer. I want to run TIM2 in trigger mode. If you connect ETR1 to Vdd, then the current at input ETR1 will be 45 mA. If you connect it to Vdd through a resistor, then the timer does not work. Where can I find a diagram of the correct connection of the trigger source? Why is there so much current in this mode?

0690X00000BvpCQQAZ.png

This topic has been closed for replies.

8 replies

waclawek.jan
Super User
Jan 10, 2020 8:43 AM UTC

> If you connect ETR1 to Vdd, then the current at input ETR1 will be 45 mA

Something is terribly wrong.

Do you have CH1 set as input (i.e. capture)? Read out and check/post the content of relevant GPIO and TIM registers.

What board is this? Isn't there something external connected to the same pin?

I don't use Cube/CubeMX.

JW

MKhan.1
MKhan.1Author
Associate
Jan 10, 2020 8:58 AM UTC

No, nothing else is connected to this contact. And if you use this pin as a simple GPIO input, then the current will be normal.0690X00000BvpM1QAJ.png

0690X00000BvpMBQAZ.png

berendi
Principal
Jan 10, 2020 8:58 AM UTC

45 mA is way too much for any I/O pin to handle, see absolute maximum ratings in the datasheet. Consider your MCU damaged, and get a replacement. This is most certainly a hardware problem, unless PA0 is somehow set as output. The setup looks right to me, but I don't trust CubeMX anymore even to get the pin setup right, so check the GPIOA registers against the reference manual.

Check the board for defects, bad soldering, etc. Use a genuine debug adatpter instead of cheap aftermarket clones if your Vdd is lower than 3.3V.

waclawek.jan
Super User
Jan 10, 2020 9:01 AM UTC

As I've said above, you have to set CH1 to input - note that PA0 is shared between ETR and CH1.

You have TIMx_CCMR1.CC1S=0b00, i.e. output (compare). Maybe it would be enough not to enable it by setting TIMx_CCER.CC1E.

JW

MKhan.1
MKhan.1Author
Associate
Jan 10, 2020 10:31 AM UTC

Thanks! Everything worked with this setting.0690X00000BvpkhQAB.png

But is there an appnote where you can read about setting up timers in CubeMx.

berendi
Principal
Jan 10, 2020 11:00 AM UTC

> But is there an appnote where you can read about setting up timers in CubeMx.

Haven't found any yet.

There are a couple of application notes on timers, dealing with advanced use cases, using the register interface.

The register interface is extensively documented in the reference manual, with step-by step instructions in the timer feature description chapter, and code examples for simpler use cases in Appendix A.

Using CubeMX is rather trial-and-error, or you must examine the generated code, look into HAL function calls, follow #defines to arrive at the actual peripheral register bit definitions to finally be able to look up in the reference manual what the generated code is actually doing.

berendi
Principal
Jan 10, 2020 10:46 AM UTC

So the cube has enabled CH1 output when it shouldn't (or is the code touching TIM2 CH1 elsewhere?). Lets fix that, using the timer without HAL.

TIM2->SMCR =
 TIM_SMCR_SMS_1|TIM_SMCR_SMS_2| // slave mode selection trigger mode
 TIM_SMCR_TS_0|TIM_SMCR_TS_1|TIM_SMCR_TS_2| // trigger selection external trigger (ETRF)
 0;
TIM2->CCMR1 =
 TIM_CCMR1_OC2M_2|TIM_CCMR1_OC2M_1|TIM_CCMR1_OC2M_0| // OC 2 mode PWM 2
 TIM_CCMR1_OC2PE| // preload enable - do you really need that?
 0;
TIM2->CCER = TIM_CCER_CC2E; // channel 2 output enable
TIM2->PSC = 48000 - 1;
TIM2->ARR = 2000; // timer period, didn't you mean 2000 - 1 ?
TIM2->CCR2 = 1000; // duty cycle
TIM2->EGR = TIM_EGR_UG; // activate preloaded value
TIM2->CR1 = TIM_CR1_OPM; // one pulse mode

This looks like a quite dangerous bug, which version of CubeMX and HAL do you have?

MKhan.1
MKhan.1Author
Associate
Jan 10, 2020 10:52 AM UTC

Thanks! Version 5.3.0

0690X00000BvpsbQAB.png