Question
STM32CubeIDE version 1.2.0 is now released
Hello community!
I don't plan to sticky this post, it's just planned as a small announcement to make people aware of the new version.
If you prefer that I do these for future releases and/or prefer that I do sticky these posts please let me know.
Some highlights of the new release includes:
- Target support updated in-sync with STM32Cube ecosystem in general.
- The amount of available example projects targeting STM32CubeIDE for new STM32 devices are increasing.
- Integration of STM32CubeMX 5.5.0 and STM32CubeProgrammer 2.3.0
- STM32CubeMX integration improvements
- Import of ioc-file to create new STM32CubeIDE project.
- Ioc-editor related issues on macOS solved.
- Bug fixes related to clock configuration fields in ioc-editor.
- STM32CubeMX menus, such as “Check for updates�? now also available without opening an ioc-file.
- Release build configuration now uses “–Os�? optimization by default (new projects only, old projects not touched).
- Removal of the “debug probe filter�? allows users to use selected debug probe with any MCU/Board. Sometimes with a warning message.
- Maturation of support for STM32L5 in general.
- Support for flash/debug of N-S application when RDP=0.5 with OpenOCD and ST-LINK GDB server.
- Added SVD-files and support for disableConditions.
- ST-LINK GDB server changes
- Default reset strategy changed to “connect under reset�? to simplify debug of low-power examples.
- Fixed connect bug on macOS with the new STM32CubeProgrammer version
I have also updated the sticky post "Features and known issues" to reflect version 1.2.0.
It's available here: