Skip to main content
EVoro.1
Associate
January 2, 2020
Question

Unavailable "Setting" tab and problem with make

  • January 2, 2020
  • 3 replies
  • 1015 views

Hi everybody!

Have problem with building project, which is OK in TrueStudio.

I have:

Core/Inc/font24.o:(.rodata.Font24_Table+0x0): first defined here

collect2: error: ld returned 1 exit status

make: *** [makefile:42: test3.elf] Error 1

"make -j7 all" terminated with exit code 2. Build might be incomplete.

15:42:59 Build Failed. 1 errors, 0 warnings. (took 151ms)

Tried to solve the issue with Builder setting, but this settings is unavailable under MacOS Catalina /STM32CubeICE

Could you pls suggest any solution?

Regards

Evgenii

This topic has been closed for replies.

3 replies

Markus GIRDLAND
ST Employee
January 8, 2020

Do you get that pop-up with every project you create or this specific one that worked in TrueSTUDIO?

Do you have a way to recreate the problem?

EVoro.1
EVoro.1Author
Associate
January 8, 2020

yes. Every project I've generated I had this pop up message.

Markus GIRDLAND
ST Employee
January 8, 2020

Seems like I get the same thing after some testing. I'll write a ticket about it.