2019-12-29 4:32 PM
Hi,
I`m trying to read the SDCard using FatFS and Decode the JPEG file then show on LCD, but I face some problem on it.
I reference the JPEG_DecodingUsingFs_DMA in STM32Cube_FW_H7_V1.5.0, and the detail code down below.
uint32_t JPEG_Decode_DMA(JPEG_HandleTypeDef *hjpeg, FIL *file, uint32_t DestAddress)
{
  uint32_t i;
  
  pFile = file;
  FrameBufferAddress = DestAddress;
          
  /* Read from JPG file and fill input buffers */
  for(i = 0; i < NB_INPUT_DATA_BUFFERS; i++)
  {
    if(f_read (pFile, Jpeg_IN_BufferTab[i].DataBuffer , CHUNK_SIZE_IN, (UINT*)(&Jpeg_IN_BufferTab[i].DataBufferSize)) == FR_OK)
    {
      Jpeg_IN_BufferTab[i].State = JPEG_BUFFER_FULL;
    }
    else
    {
      Error_Handler();
    }        
  } 
	
  /* Start JPEG decoding with DMA method */
	
  HAL_JPEG_Decode_DMA(hjpeg ,Jpeg_IN_BufferTab[0].DataBuffer ,Jpeg_IN_BufferTab[0].DataBufferSize ,(uint8_t *)FrameBufferAddress ,CHUNK_SIZE_OUT);
	
  return 0;
}But it can`t show all pixels on the screen only a part of them,like limited by some parameters.
This is a official code from CubeMX.
Is there anyone can help to solve or similar experience can share?
Thank you!
 
2019-12-29 5:51 PM
Make sure the file data content reads correctly, and matches integrity checks from PC. ie CRC file/content, confirm it reads properly and consistently.
Try with multiple examples.
2019-12-29 6:04 PM
Hi @Community member ,
Thanks for your reply!
I have checked the data that read from FatFS with debug simulation, and it all correct.
But I can`t promise the output data in SDRAM and on Screen like the picture bottom pixel was not right.
Is there any method can check the problem?