cancel
Showing results for 
Search instead for 
Did you mean: 

STSPIN32F0 external 3.3V power supply issue

JLi.31
Associate
  1. mode 1:SW pin short to GND or VDD,how to short ?connect direct or use resistance(what is the best value?), internal swith will not work
  2. mode 2 :SW pin NC or connect to VM,but the internal swith is working still。
  3. in high temperature ,High efficiency ,Long life condition,what is the best of two ?
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Cristiana SCARAMEL
ST Employee

​In mode 1 we suggest to connect the SW directly to GND (preferred option) to keep the internal switch latched off.

From the listed points of view there is no difference. Anyway the connection between the SW pin and GND is preferred in order to reduce the EMI.

If you feel a post has answered your question, please click "Accept as Solution"

View solution in original post

1 REPLY 1
Cristiana SCARAMEL
ST Employee

​In mode 1 we suggest to connect the SW directly to GND (preferred option) to keep the internal switch latched off.

From the listed points of view there is no difference. Anyway the connection between the SW pin and GND is preferred in order to reduce the EMI.

If you feel a post has answered your question, please click "Accept as Solution"