Associate II
December 22, 2019
Question
[STM32CubeProgrammer] failed to load external flash memory via bootloader
- December 22, 2019
- 2 replies
- 1176 views
hi i am using stm32f769 discovery board , i took one of the examples that provides with touchgfx , and everything work fine (program through st-link with STM32CubeProgrammer ) . but now i want to try to upload the program through the bootloader (with STM32CubeProgrammer ), so after erasaing the mcu and the external memory ,i succeed to connect to the bootloader and upload the software to mcu but when it getting to the external flash its failed .
and after reset of the mcu i can see the program in the screen with white boxes where the pictures should be . so its seems that mcu fine but STM32CubeProgrammer not recognzie the flash sector or some thing...
will appreciate any help
thanks