Skip to main content
Trevor Jones
Senior
Dec 19, 2019 2:36 AM UTC
Question

H743 USB Host

I have the Keyboard working,

but when a usb hub is installed the keyboard is not visible

does anyone have some clues to get a usb hub working ?

This topic has been closed for replies.

14 replies

Tesla DeLorean
Guru
Dec 19, 2019 4:03 PM UTC

@Camilo LEMOS​  recurrent issues with ST USB IP and hubs

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Camilo LEMOS
Associate II
Dec 19, 2019 4:13 PM UTC

Thanks for letting me know Clive! I have just brought this to our support team (extending to product team as well) to see how we can best address the recurrent issue. I (or another member of the team, with more knowledge than me on this topic) will post back here as soon as we have more info.

Pavel A.
Dec 19, 2019 8:51 PM UTC

> does anyone have some clues to get a usb hub working ?

On the Segger forum (they sell a commercial USB library) someone reported success connecting a hub to STM32F407 eval.board.

We could not reproduce this, but this may be our fault.

YMMV.

We also started to adapt this hub example to a custom board with STM32F446. It basically worked with a FS hub, but we have not finished this.

-- pa

waclawek.jan
Super User
Dec 19, 2019 10:09 PM UTC

> On the Segger forum (they sell a commercial USB library) someone reported success connecting a hub to STM32F407 eval.board.

Do you have any link?

JW

waclawek.jan
Super User
Apr 11, 2023 9:20 AM UTC

Hi @Community member​ ,

sorry for resurrecting an old thread, but I wonder if you were successful in running hub on the 'H7 USB with internal PHY, i.e. if the Host packet transmission may hang when connecting through a hub to a low-speed device erratum has been fixed for the 'H7.

Thanks,

JW

Trevor Jones
Senior
Apr 11, 2023 11:06 AM UTC

Hello Jan, Pavel, Clive... long time no see... @Pavel A. @waclawek.jan @Community member​ 

Jan, no sorry, I never got it going, just too difficult...

the call stack is the easy bit, making the calls work is where I came unstuck.

got Host running ok, CDC of course, all DMAs, all easy... but the HUB was just crazy... hoping ST has improved the resources now after a couple of years.. I know Pavel has had some success with that.

Would like to get it running.

Willing to try again if you wish... might need support from you guys.

Got my shiny new STM32U5A9J-DK last week... could try on that if you wish... although the DMA systems are significantly different on this chip.

Have you seen the spec on this new chip ? 2.5MBytes of Ram... and a 2Lane DSI port...

still not enough for a decent display size... just cant bring myself to run a small 400x320 display..

I have many kits here just let me know which one you would like to use..

the local FAE is saying the chip is going to be very well priced.

Hey Pavel, which chip are you using for displays ?

Do you have a HUB solution ?, I could port it over if you would like...

Nick.

Pavel A.
Apr 11, 2023 12:11 PM UTC

Hi @Community member​ one active project uses the same LCD, or compatible, as on the 32F746GDISCOVERY board. I don't have the exact part ID. Another projects use cheap matrix LCD (not graphics).

About USB hub, my former customer went for the Segger library and is happy with it AFAIK.

I have not finished that thing to product state.

They also told me about their competitor that managed to develop a FS hub support and host driver themselves. Their use case is quite limited though, not pushing the USB to the edge.

Trevor Jones
Senior
Apr 11, 2023 12:29 PM UTC

Thanks Pavel, Jan

waclawek.jan
Super User
Apr 11, 2023 11:52 AM UTC

Oh, so HUB is still no go... Thanks.

JW

Trevor Jones
Senior
Apr 11, 2023 12:02 PM UTC

now that there is 2.5MBytes Ram, it could be useful..

if you get some work going, please let me know.

happy to cooperate with someone.