Skip to main content
ASaee.1
Associate
Dec 18, 2019 11:09 AM UTC
Question

STEVAL-IDP004V1 USB Function: Unable to determine what function does the usb port on the I/O Link board serves.

..

    This topic has been closed for replies.

    1 reply

    Winfred LU
    ST Employee
    Dec 27, 2019 3:10 AM UTC

    USB, RS-485, and CAN on the STEVAL-IDP004V1 are provided for more flexibility, which can be used for data exchange with additional units and with multiple sensor connections on the STEVAL-IDP003V1.

    In the evaluation firmware, PC_Communication_USB project is to manage command decoding and data exchange between the STEVAL-IDP004V1 and a PC.