Skip to main content
SR.1498
Visitor II
December 18, 2019
Question

LSM6DS3TR-C thermal charactersitics.

  • December 18, 2019
  • 1 reply
  • 1144 views

Please share the below details for LSM6DS3TR-C,

1. Junction to ambient thermal resistance?

2. Junction to case thermal resistance?

3. Maximum operating case temperature?

4 .Maximum operating junction temperature?

This topic has been closed for replies.

1 reply

Eleon BORLINI
ST Employee
December 19, 2019

Hi @SR.1498​ , for which application do you need these details? Pls consider that the LSM6DS3TR max supply is 3.6V and max current (high performance mode, max ODR) is 1250uA, so the power consumed in the worst case is P=V*I=4,5mW. If you consider that the device package thermal resistance is typ 80°C/W, the thermal difference between the device and the environment is DeltaT=0.3°C worst case. The maximum operating junction is basically the abs max rating in the datasheet. Regards