Skip to main content
Dimitris Paraskevopoulos
Associate III
December 18, 2019
Question

AN4826 Errors

  • December 18, 2019
  • 0 replies
  • 423 views

There are a couple of inconsistencies in AN4826.

First one that has been repeated in other posts is that there is a bug in the bootloader and BOOT0 pin's state is actually irrelevant as it always boots from BOOT_ADD0 anyway.

So the select BOOT_ADDx based on BOOT0 pin does not exist. Also there seems to be a footnote missing there.

Second one is that in Figure 9 it says that when nDBOOT=0 it will boot from RAM if boot address is in RAM however in Figure 10 this points to a state which says "Jump to AXIM-Flash base address 0x0800 0000"

Another question that I have is whether the following statement is correct

"nWRP[i] bit is write protection bit for sector(2*i) and sector (2*i+1)"

Is that the intention. I was thinking that maybe we may want to write protect respective sectors in both banks so sector 0 and 12 together, 1 and 13 etc.

Can someone from ST please confirm?

Thank you.

This topic has been closed for replies.