Skip to main content
SKein.1
Visitor II
December 12, 2019
Question

LIS3DH using too much power on custom board

  • December 12, 2019
  • 1 reply
  • 875 views

I have a custom board that includes the LIS3DH. With the LIS3DH not populated, my board uses 0.009mA, but with the LIS3DH populated and not configured, it uses 0.135mA.

According the data sheet, it should be 0.011mA. The data sheet also says the LIS3DH is set to "Power Down Mode" by default.

Attached is the schematic of the LIS3DH on my custom board. Is it not connected correctly?

0690X00000BuYGJQA3.png

The pseudo-code to turn the LIS3DH off is:

LIS3DH_ADDRESS = 0x18 ;

REG1_REG = 0x20; //REG_1

REG1_VALUE = 0x00;

LIS3DH_WriteReg(LIS3DH_ADDRESS, REG1_REG, REG1_VALUE);

-- this is still using too much power.

Is it a software problem or hardware?

thank you,

Steve

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    December 13, 2019

    Hi Steve, I think that it could be mainly related to an HW root cause. The datasheet says at p.9: SDO/SA0 pin is internally pulled up. Refer to Table 3 for the internal pull-up values (typ.). If you connect the SDO pin to GND you create a path (even if not direct) from VBAT to GND causing an over-current consumption. Regards