Skip to main content
Gpeti
Senior
December 10, 2019
Question

Not possible to connect to STM32H7 in RDP level 1 through CubeProgrammer without disabling RDP

  • December 10, 2019
  • 2 replies
  • 1000 views

I'm implementing in my firmware on STM32H7 the change of RDP Level.

In RDP Level 1, I can still connect through ST USB bootloader by setting signal BOOT0 (as expected). However when I connect to STM32CubeProgrammer, it asks if I want to disable RDP: it's not possible to access the chip memory without doing a regression to Level 0. I don't understand why: the ref manual says that in RDP 1, the STM32 bootloader from system memory is limited to a few commands but actually it can also modify the option byte to do a regression to level 0 so it is not perfectly clear.

This topic has been closed for replies.

2 replies

Piranha
Principal III
December 10, 2019

You are using RDP, but do you know what that RDP abbreviation means?

Gpeti
GpetiAuthor
Senior
December 10, 2019

OK you're right, my question was stupid, I was confused by the capability of STM32 bootloader, I edited the answer (since I cannot delete it)