Skip to main content
DCook.2270
Visitor II
December 7, 2019
Question

Would like to use STNRGPF01 Digital Controller for a system with 480 VAC input. The AC input voltage sensing is isolated, is there a reason this can't be used at 480 VAC?

  • December 7, 2019
  • 0 replies
  • 643 views

When trying to set up a simulation in E-Design, the highest input voltage that can be input is 265?

If this can be used at 480 VAC as I suspect, how do I get the voltage settings on the E-desgn tool revised

This topic has been closed for replies.