2019-12-06 5:52 AM
My STM32H7 firmware was working and compiling fine before I upgrade my CubeMX firmware package from 1.3.0 to 1.5.0.
It seems that the GPIO register struct has been changed and "BSRRH" and "BSRRL" members of the struct do not exist anymore! So my code does not compile! What should I do? E.g. code below:
CTRL_N3_GPIO_Port->BSRRL = CTRL_N1_Pin; // SET
CTRL_N3_GPIO_Port->BSRRH = CTRL_N2_Pin; // RESETThe error is:
Field 'BSRRH' could not be resolved main.c
The struct now only offers "BSRR". How can I solve this problem and why even such major changed made its way into this patch?
Solved! Go to Solution.
2019-12-06 6:00 AM
CTRL_N3_GPIO_Port->BSRR = (uint16_t)CTRL_N1_Pin; // SET
CTRL_N3_GPIO_Port->BSRR = (uint16_tCTRL_N2_Pin << 16; // RESET
> why even such major changed made its way into this patch?
Maybe 16-bit accesses to high and low parts of BSRR do not work in some cases. 32-bit access always works.
1.5.0 is not a patch, btw, it is a major version. Patches are denoted by the 3rd number (Z in X.Y.Z).
-- pa
2019-12-06 6:00 AM
CTRL_N3_GPIO_Port->BSRR = (uint16_t)CTRL_N1_Pin; // SET
CTRL_N3_GPIO_Port->BSRR = (uint16_tCTRL_N2_Pin << 16; // RESET
> why even such major changed made its way into this patch?
Maybe 16-bit accesses to high and low parts of BSRR do not work in some cases. 32-bit access always works.
1.5.0 is not a patch, btw, it is a major version. Patches are denoted by the 3rd number (Z in X.Y.Z).
-- pa
2019-12-06 10:49 AM
Thanks Pavel.
I knew the solution is to shift bits. My point was how to do it in the struct to fix it in one place only (I have hundreds of BSRRX in my code).
But now that you say it is a major release then I will revert back to 1.3.Z and save myself some time :))
2019-12-07 1:14 AM
This is why people create and use APIs. Even, when not using functions, at least make some simple macros. For example:
You'll be able to change macro's underneath functionality easily and not need those code comments anymore, as macro's name already says what it does.