Skip to main content
Taxara
Associate III
December 6, 2019
Solved

What is the fastest adc sampling speed when using 4 adc's

  • December 6, 2019
  • 7 replies
  • 2830 views

Hi

I thinking of buying and STM32WB (P-NUCLEO-WB55 evaluation board) because of the fast ADC.

I need to sample four analog signals with a rate of a few hunderd Ksps and store their values.

  • what would roughly be the sample rate when using 4 adc inputs (8bit)?
  • Is there any direction you can guide me to, to accomplish this? (example/ adc application note)

Thanks in advance,

This topic has been closed for replies.
Best answer by Philippe Cherbonnel

Hello,

As said above by Remi, the ADC is fast enough for your " few hunderd Ksps" application, you can even use it with resolution 12 bits.

You can refer to STM32WB reference manual for conversion time calculation.

conversion time = (sampling time + conversion time resolution) x (1/ ADC clock freq)

for example, with ADC resolution 12 bits, sampling time 47.5 ADC clock cycles, ADC clock freq 64MHz:

conversion time = 0.9375us <=> 1Msmp/sec

About examples to help you start your application:

There are several examples in STM32WB FW package (available to download on www.st.com).

Here are some examples using multiple ADC channels:

  • using ADC LL driver:

...\Firmware\Projects\P-NUCLEO-WB55.Nucleo\Examples_LL\ADC\ADC_GroupsRegularInjected_Init

Convert one channel with trigger from timer and data transfer by DMA, another channel on asynchronous trigger

  • using ADC HAL driver:

...\Firmware\Projects\P-NUCLEO-WB55.Nucleo\Examples\ADC\ADC_MultiChannelSingleConversion

Convert 3 channels (1 from GPIO and 2 internals (VrefInt, internal temperature sensor)) with data transfer by DMA.

Best regards

Philippe

7 replies

Ozone
Principal
December 6, 2019

The datasheet for the STM32WB55CC says 4,26 Msps.

Up to 7,11 Msps with reduced resolution.

Taxara
TaxaraAuthor
Associate III
December 6, 2019

Yes this seems to be the case when using one adc. But i think, (i cant really find this) that it would be divided by x when sampling x at the same time.

TDK
December 6, 2019

Yes, it will be x/4 if you use a single adc. Or x/2 if you use two adcs for 2 channels each. If that chip has two adcs. Still gets you well over a couple hundred ksps in either case.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Remi QUINTIN
ST Technical Moderator
December 9, 2019

​For 8 bit resolution , the fast ADC of the STM32WB can achieve up to 5.81 Msps. This let over 1.4 Msps for each of the 4 signals.

It is by far enough for the signals you want to sample.

Philippe Cherbonnel
ST Employee
December 20, 2019

Hello,

As said above by Remi, the ADC is fast enough for your " few hunderd Ksps" application, you can even use it with resolution 12 bits.

You can refer to STM32WB reference manual for conversion time calculation.

conversion time = (sampling time + conversion time resolution) x (1/ ADC clock freq)

for example, with ADC resolution 12 bits, sampling time 47.5 ADC clock cycles, ADC clock freq 64MHz:

conversion time = 0.9375us <=> 1Msmp/sec

About examples to help you start your application:

There are several examples in STM32WB FW package (available to download on www.st.com).

Here are some examples using multiple ADC channels:

  • using ADC LL driver:

...\Firmware\Projects\P-NUCLEO-WB55.Nucleo\Examples_LL\ADC\ADC_GroupsRegularInjected_Init

Convert one channel with trigger from timer and data transfer by DMA, another channel on asynchronous trigger

  • using ADC HAL driver:

...\Firmware\Projects\P-NUCLEO-WB55.Nucleo\Examples\ADC\ADC_MultiChannelSingleConversion

Convert 3 channels (1 from GPIO and 2 internals (VrefInt, internal temperature sensor)) with data transfer by DMA.

Best regards

Philippe

Taxara
TaxaraAuthor
Associate III
December 20, 2019

Hi Philippe

Thanks for the examples and extensive information!

Cheers,

Taxara