Question
Power consumption of the Nucleo 64 board : STM32L073ZR.
Hi everyone!
I am trying to get the lowest power consumption from the STM32L073ZR in STOP Mode.
I run my tests with the board powered from external source E5V (no USB connected).
I have two Ampere-meters:
- one measure the current IDD of the microcontroller (JP6)
- the other measure the overall consumption of the board
I get IDD = 0.3 uA (so i enter the STOP Mode correctly). However i measure 50 mA for the total current.
Do someone knows where the 50 mA come from and how to reduce it?
Nb: I didn't touch any solder bridge yet.