Skip to main content
Evgeny Sobolev
Associate II
December 2, 2019
Solved

STM32F4xx USB bug, when compiled by GCC using -O3 option.

  • December 2, 2019
  • 3 replies
  • 2051 views

Setup:

Project, generated by CubeMX and compiled by arm-none-eabi-gcc-9.2.0 toolchain.

CubeMX firmware package version: STM32Cube FW_L4 V1.14.0

CPU: STM32L432KCY (and others)

Toolchain: arm-none-eabi-gcc-9.2.0 (and others)

Compiler options: -mcpu=cortex-m4 -mthumb -mfloat-abi=softfp -mfpu=fpv4-sp-d16 -O3 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -fno-inline-functions

Problem:

Usb not working properly.

0690X00000AtA3eQAF.jpg

Solution:

FunctionUSB_WritePMA, not working properly when project compiled using -O3 optimization option. Let's look at the file stm32l4xx_ll_usb.c. Pls. look at the function

/**
 * @brief Copy a buffer from user memory area to packet memory area (PMA)
 * @param USBx USB peripheral instance register address.
 * @param pbUsrBuf pointer to user memory area.
 * @param wPMABufAddr address into PMA.
 * @param wNBytes: no. of bytes to be copied.
 * @retval None
 */
void USB_WritePMA(USB_TypeDef *USBx, uint8_t *pbUsrBuf, uint16_t wPMABufAddr, uint16_t wNBytes)
{
 uint32_t n = ((uint32_t)wNBytes + 1U) >> 1;
 uint32_t BaseAddr = (uint32_t)USBx;
 uint32_t i, temp1, temp2;
 uint16_t *pdwVal; // Fix: make it volatile // volatile uint16_t *pdwVal;
 uint8_t *pBuf = pbUsrBuf;
 
 pdwVal = (uint16_t *)(BaseAddr + 0x400U + ((uint32_t)wPMABufAddr * PMA_ACCESS));
 
 for (i = n; i != 0U; i--)
 {
 temp1 = (uint16_t) * pBuf;
 pBuf++;
 temp2 = temp1 | ((uint16_t)((uint16_t) * pBuf << 8));
 *pdwVal = (uint16_t)temp2;
 pdwVal++;
 
#if PMA_ACCESS > 1U
 pdwVal++;
#endif
 
 pBuf++;
 }
}
volatile uint16_t *pdwVal;

After fix:

0690X00000AtA4cQAF.jpg

This topic has been closed for replies.
Best answer by Imen.D

Hello @Evgeny Sobolev (Community Member)​ ,

This issue will be fixed in the next release of STM32CubeL4 V1.15.

So, please keep an eye out for the next update!

Thank you for highlighting this issue.

Best Regards,

Imen

3 replies

Imen.DBest answer
ST Technical Moderator
December 2, 2019

Hello @Evgeny Sobolev (Community Member)​ ,

This issue will be fixed in the next release of STM32CubeL4 V1.15.

So, please keep an eye out for the next update!

Thank you for highlighting this issue.

Best Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Evgeny Sobolev
Associate II
December 2, 2019

Please don't forget to fix it on another controller families.

Thanks.

Dave Nadler
Senior III
December 19, 2019

@Evgeny Sobolev​ - Thanks for the fix.

Can you explain what the compiler did that using volatile solves?

While that code obviously leaves plenty of room for improvement, I don't see any obvious aliasing or other coding errors?

Thanks!

Best Regards, Dave