Skip to main content
Renato
Associate
November 29, 2019
Solved

STM32F030F4P6 PWM on PA4 not working

  • November 29, 2019
  • 2 replies
  • 1352 views

Hi,

I've set up a PWM with TIM14_CH1 on pin PB1, using standard peripherial library and this worked fine (the signal on the output-pin was just as expected).

Now I've tried to move the PWM signal from pin PB1 to PA4, still using TIM14_CH1, but with no success (the pin stays low, no pwm signal at all).

Here is the code is used (:

	// PWM (Tim14)
	//-------------
 
	// GPIOx Clock enable
	RCC_AHBPeriphClockCmd( RCC_AHBPeriph_GPIOB, ENABLE);
//RCC_AHBPeriphClockCmd( RCC_AHBPeriph_GPIOA, ENABLE);
 
	// GPIOx Pin configure (as alternate function push-pull)
	GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1;
//GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;
	GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
	GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
	GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
	GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
	GPIO_Init(GPIOB, &GPIO_InitStructure);
	GPIO_PinAFConfig(GPIOB, GPIO_PinSource1, GPIO_AF_0);
//GPIO_Init(GPIOA, &GPIO_InitStructure);
//GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_0);
 
	// TIM14 clock enable
	RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM14 , ENABLE);
 
	// calc PWM-Periode (102 kHz)
	PWM_period = (SystemCoreClock / 102000 ) - 1;
 
	// calc PWM-DutyC pulse (50% Dutycycle)
	PWM_DutyC_pulse = ((PWM_period- 1) / 2);
 
	// Time Base configure
	TIM_TimeBaseStructure.TIM_Prescaler = 0;
	TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
	TIM_TimeBaseStructure.TIM_Period = PWM_period;
	TIM_TimeBaseStructure.TIM_ClockDivision = 0;
	TIM_TimeBaseStructure.TIM_RepetitionCounter = 0;
	TIM_TimeBaseInit(TIM14, &TIM_TimeBaseStructure);
 
	// Timer compare-channel 1 configure (in PWM mode)
	TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1;
	TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
	TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Disable;
	TIM_OCInitStructure.TIM_Pulse = 0;
	TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
	TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCNPolarity_Low;
	TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Set;
	TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCIdleState_Reset;
	TIM_OC1Init(TIM14, &TIM_OCInitStructure);
 
	// Timer enable
	TIM_Cmd(TIM14, ENABLE);
 
	// Timer PWM output enable
	TIM_CtrlPWMOutputs(TIM14, ENABLE);
 
	// start PWM (set DutyC > 0)
	TIM_SetCompare1(TIM14, PWM_DutyC_pulse);

This topic has been closed for replies.
Best answer by waclawek.jan

> //GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_0);

Note, that on PA4, TIM14_CH1 is *not* AF0 but AF4.

JW

2 replies

waclawek.jan
waclawek.janBest answer
Super User
January 16, 2020

> //GPIO_PinAFConfig(GPIOA, GPIO_PinSource4, GPIO_AF_0);

Note, that on PA4, TIM14_CH1 is *not* AF0 but AF4.

JW

Renato
RenatoAuthor
Associate
January 24, 2020

Thank you very much for the hint.

This solved my Problem and everything is no working as expected. Knowing what was wrong, I now could also find the Information inside the Chip datasheet.

Quite unbelievable that it did not occur to me to check the alternate function when I changed the pin.