Skip to main content
LRicc.1843
Associate
Nov 29, 2019 11:09 AM UTC
Question

How can I make SensorTile and my Computer communicate through BLE?

Hi, for my thesis, I am doing a project with SensorTile (STEVAL-STLKT01V1), and I am trying to let him communicate with my computer (I have Windows 10), but until now I have only been able to pair the SensorTile with my computer. I followed the UCLA tutorials, but about the BLE communication they use only Linux. Can anyone help me?

This topic has been closed for replies.

4 replies

Winfred LU
ST Employee
Dec 2, 2019 3:22 AM UTC

The BLE does not differentiate different OSes.

Did you mean to use BlueZ under Linux?

LRicc.1843
Associate
Dec 2, 2019 8:02 AM UTC

I must build an application in windows 10 able to acquire and plot all the outputs of SensorTile, and I was wonderinf if there is any basic application or system that I can use to start without Linux.

Rita Ch.
Associate II
Dec 3, 2019 11:13 PM UTC

+1 I would be very interested to hear the answer. I need to build a Windows application that would read and process data from a SensorTile over the air. I would really like to avoid any solid cable connection to the sensorTile because it's a very vibration-sensitive application (telescope guidance). So far I did not find a way to do it. It is obviously possible because Unicleo does it somehow, but the SDKs I was able to find (BlueST and BlueZ) support only Linux-based platforms. I guess it would be possible to run a Linux app on Windows in a VM, but it seems a bit bulky for a good solution.

Many thanks!

Winfred LU
ST Employee
Dec 4, 2019 3:43 AM UTC

For Windows app development, please refer to Microsoft online document:

https://docs.microsoft.com/en-us/windows/uwp/devices-sensors/bluetooth-low-energy-overview

You may be interested in this:

https://blogs.msdn.microsoft.com/cdndevs/2017/04/28/uwp-working-with-bluetooth-devices-part-1/

And together with the sample code:

Chapter26_BluetoothData on https://github.com/sbaidachni/Win10BookSamples