When I generate code I get a popup that says "- These IPs still have some not configured or wrong parameter values:[GFXSIMULATOR] Do you still want to generate the code ? Yes/No
I check yes and everything appears to work.
What is the GFXSIMULATOR mode and can I deselect it in the Pinout & Configuration tab?
I see the generated code in main.c calls a generated init function, but it is empty except for comments delineating user code sections.
When I select Pinout & Configuration tab -> Application -> GFXSIMULATOR, it says the FAHB (MHz) is configured for 180 but the simulator is 168. All the other configuration settings match the simulator settings. I suspect this is the cause of the popup. But I want to run at 180. How should I proceed?
Thank you,