Skip to main content
JParm.1325
Associate II
November 15, 2019
Question

Ping with freeRTOS and lwIP configuration

  • November 15, 2019
  • 2 replies
  • 1444 views

Hey there,

I am using an STM32F767ZIT6 and I am not realy an advanced programmer. The IDE I am using is STM32CubeIDE v1.1.0 .

When I create a new Project, I use the pinout configuration to initialize freeRTOS, ETH and lwIP. At System Core I changed the Timebase Source to a Timer. Also I change the clock configuration to 216 MHz, cause of ETH. In lwIP I disable DHCP and use a static IP. So far so good.

All other configurations are on default. Now I connect my Nucleo 144 to my PC and try to Ping, but nothing happend, no communication.

When debugging this project, I stuck in the lwIP init.

Are there any other configurations I need to do, to Ping my Board?

This topic has been closed for replies.

2 replies

JParm.1325
Associate II
November 15, 2019

Me again,

I changed the Stack Size of the Task to 1024. Through this change, i do not stuck in the lwIP init anymore.

But still can not ping.

JParm.1325
Associate II
November 18, 2019

The "PHY Address" value must be set to 0. Also the IDE pinout configuration connect two false pins. PG11 and PG13 must be set manuel to ETH_TX_EN and ETH_TXD0 !

Now the Ping worked!