Skip to main content
ambinabhi
Associate II
November 13, 2019
Question

HO to put STM32 IoT node into deep sleep and wake up every hour from alarm clock.

  • November 13, 2019
  • 0 replies
  • 616 views

HI

I am using the STM32L475 IoT discovery kit, I want put my board into deep sleep and wake up every one hour based on event, I was considering setting up alarm clock. I am using x-cube-cld-gen library'r MQTT example.

For now i have scene other examples and set up the alarm sample code. But i don't get the HAL_RTC_AlarmAEventCallback trigger. The clock just keeps on running.

/* Configure the system clock */
 SystemClock_Config();
 
 Periph_Config();
 
 BSP_LED_Init(LED_GREEN);
 // BSP_PB_Init(BUTTON_USER, BUTTON_MODE_EXTI);
 
 /* RNG init function */
 hrng.Instance = RNG;
 if (HAL_RNG_Init(&hrng) != HAL_OK)
 {
 Error_Handler();
 }
 
 /* UART console init */
 Console_UART_Init();
 
 hrtc.Instance = RTC;
 /* RTC init */
 RTC_Init();
 RTC_AlarmConfig();
 
#ifdef FIREWALL_MBEDLIB
 firewall_init();
#endif
 
 while(1){
	 RTC_TimeShow(aShowTime);
	 if(wake_up_time){
		 printf("I woke up on time....\r\n");
	 }
	 HAL_Delay(1000);
 }
void Periph_Config(void)
 {
 RCC_PeriphCLKInitTypeDef PeriphClkInit;
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_RTC|RCC_PERIPHCLK_USART1
 |RCC_PERIPHCLK_USART3|RCC_PERIPHCLK_I2C2
 |RCC_PERIPHCLK_RNG;
 PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2;
 PeriphClkInit.Usart3ClockSelection = RCC_USART3CLKSOURCE_PCLK1;
 PeriphClkInit.I2c2ClockSelection = RCC_I2C2CLKSOURCE_PCLK1;
 PeriphClkInit.RngClockSelection = RCC_RNGCLKSOURCE_MSI;
 
 PeriphClkInit.RTCClockSelection = RCC_RTCCLKSOURCE_LSE;
 
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 Error_Handler();
 }
 
 __HAL_RCC_PWR_CLK_ENABLE();
 
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
 {
 Error_Handler();
 }
}
static void RTC_Init(void)
{
 /**Initialize RTC Only */
 hrtc.Instance = RTC;
 hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
 hrtc.Init.AsynchPrediv = 0x7F;
 hrtc.Init.SynchPrediv = 0xF9;
 hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
#ifdef RTC_OUTPUT_REMAP_NONE
 hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
#endif
 hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
 hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
 if (HAL_RTC_Init(&hrtc) != HAL_OK)
 {
 Error_Handler();
 }
}
static void RTC_AlarmConfig(void)
{
 printf("Setting alarm...\r\n");
 RTC_DateTypeDef sdatestructure;
 RTC_TimeTypeDef stimestructure;
 RTC_AlarmTypeDef salarmstructure;
 
 /*##-1- Configure the Date #################################################*/
 /* Set Date: Tuesday February 18th 2014 */
 sdatestructure.Year = 0x14;
 sdatestructure.Month = RTC_MONTH_FEBRUARY;
 sdatestructure.Date = 0x18;
 sdatestructure.WeekDay = RTC_WEEKDAY_TUESDAY;
 
 if(HAL_RTC_SetDate(&hrtc,&sdatestructure,RTC_FORMAT_BCD) != HAL_OK)
 {
 /* Initialization Error */
 Error_Handler();
 }
 
 /*##-2- Configure the Time #################################################*/
 /* Set Time: 02:20:00 */
 stimestructure.Hours = 0x02;
 stimestructure.Minutes = 0x20;
 stimestructure.Seconds = 0x00;
 stimestructure.TimeFormat = RTC_HOURFORMAT12_AM;
 stimestructure.DayLightSaving = RTC_DAYLIGHTSAVING_NONE ;
 stimestructure.StoreOperation = RTC_STOREOPERATION_RESET;
 
 if(HAL_RTC_SetTime(&hrtc,&stimestructure,RTC_FORMAT_BCD) != HAL_OK)
 {
 /* Initialization Error */
 Error_Handler();
 }
 
 /*##-3- Configure the RTC Alarm peripheral #################################*/
 /* Set Alarm to 02:20:30
 RTC Alarm Generation: Alarm on Hours, Minutes and Seconds */
 salarmstructure.Alarm = RTC_ALARM_A;
 salarmstructure.AlarmDateWeekDay = RTC_WEEKDAY_MONDAY;
 salarmstructure.AlarmDateWeekDaySel = RTC_ALARMDATEWEEKDAYSEL_WEEKDAY;
 salarmstructure.AlarmMask = RTC_ALARMMASK_DATEWEEKDAY;
 salarmstructure.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_NONE;
 salarmstructure.AlarmTime.TimeFormat = RTC_HOURFORMAT12_AM;
 salarmstructure.AlarmTime.Hours = 0x02;
 salarmstructure.AlarmTime.Minutes = 0x20;
 salarmstructure.AlarmTime.Seconds = 0x30;
 salarmstructure.AlarmTime.SubSeconds = 0x56;
 
 if(HAL_RTC_SetAlarm_IT(&hrtc,&salarmstructure,RTC_FORMAT_BCD) != HAL_OK)
 {
 /* Initialization Error */
 Error_Handler();
 }
}
void HAL_RTC_AlarmAEventCallback(RTC_HandleTypeDef *hrtc)
{
 /* Turn LED2 on: Alarm generation */
 wake_up_time = true;
 BSP_LED_On(LED2);
}

I was using the STM32L476G-EVAL's RTC_Time project as reference from the stm32cubel4 library samples.

This topic has been closed for replies.