Skip to main content
Yannek
Associate III
November 12, 2019
Solved

SPC5Studio does not allow to select receive pin for CANFlex0

  • November 12, 2019
  • 2 replies
  • 1275 views

Hello,

I am configuring pin map for SPC560B50L1. I expect to configure pins 14 and 15 as CANFlex0 TX and RX respectively.

Due to manual, pin 15 is the one for CAN-RX for my 64-pin UC:

0690X00000ArxglQAB.png

But this pin has no other option to select than SIUL/GPIO17:

0690X00000ArxgvQAB.png

For another CANbus (CANFlex3) there is an option CAN3RX for the pin 62, so I think it is a bug of SPC5Studio, isn't it? Or am I doing something wrong?

0690X00000ArxhKQAR.png

Best Regards,

Yannek

    This topic has been closed for replies.
    Best answer by Erwan YVIN

    hello ,

    It is not a bug.

    For PB[1] , CAN0RX is an intrinsec function .. you have to set in Digital Input.

    Best Regards

    Erwan

    2 replies

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    November 13, 2019

    hello ,

    It is not a bug.

    For PB[1] , CAN0RX is an intrinsec function .. you have to set in Digital Input.

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    Yannek
    YannekAuthor
    Associate III
    November 18, 2019

    Thank you, Erwan