Skip to main content
vinodstanur
Associate II
November 12, 2019
Question

Stm8s003 crashing or resetting occasionally when using halt() + GPIO ISR wakeup

  • November 12, 2019
  • 0 replies
  • 954 views
#include "stm8s.h"
 
//My delay for testing. Calibrated for milli seconds.
 
void delay2(uint16_t ms)
{
	volatile uint16_t a = 100;
	while(ms--) {
		a = 1800;
		while(a--);
	}
}
 
void main(void)
{ 
 //CLK_DeInit();
	CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1);
 
 /* Clock divider to HSI/1 */
 //CLK_SYSCLKConfig(CLK_PRESCALER_CPUDIV128);
 
 //CLK_ClockSwitchConfig(CLK_SWITCHMODE_MANUAL, CLK_SOURCE_LSI, DISABLE, CLK_CURRENTCLOCKSTATE_DISABLE);
 
 	/* Initialize LEDs in Output Push-Pull Mode */
 GPIO_Init(LED_PORT, (LED_PIN), GPIO_MODE_OUT_PP_LOW_FAST);
 
 /* Initialize PB0 (BUTTON) in Input Pullup Mode with Interrupt */
 GPIO_Init(BUTTON_PORT, BUTTON_PIN, GPIO_MODE_IN_PU_IT);
 
 /* Initialize the Interrupt sensitivity */
	EXTI_DeInit();
 
 EXTI_SetExtIntSensitivity(EXTI_PORT_GPIOC, EXTI_SENSITIVITY_FALL_ONLY);
 EXTI_SetTLISensitivity(EXTI_TLISENSITIVITY_FALL_ONLY);
 enableInterrupts(); //GPIO ISR is not populated because I am using it to just wakeup CPU.
	 
 
	int i;
	for( i = 0; i < 10; i++) { //RESET DETECTION CODE 
	 GPIO_WriteLow(LED_PORT,LED_PIN);
 delay2(100);		
	 GPIO_WriteHigh(LED_PORT,LED_PIN);
 delay2(100);		
	}
 
 //APPLICATION TEST CODE TO FIND RESET BUG. It is toggling the LED on button click, but occasionally chip is getting reset. 
 while(1) { //CHIP IS RESETTING OCCASIONALLY WHILE I am continuously triggering the button !!!! I don't know why... 
 halt(); //Push button press will wake it up.
 GPIO_WriteLow(LED_PORT,LED_PIN); //Ignoring debounce while testing...
 halt(); //Push button press will wake it up.
 GPIO_WriteHigh(LED_PORT,LED_PIN); //Ignoring debounce while testing...
 }
 
}
 

I haven't changed any option bytes and what ever is there by default is still there.

Also I haven't configured any watchdog and I am not finding any watchdog reset issue because if I am not pressing the button, the LED state is not changed that means the chip is not resetting. But while I am pressing the button, one out of 10 time or one out of 20 times it resets the chip. I haven't configured anything before using halt() feature, I just measured the current at default halt mode and I am okay with it, so I just continued using it. But now I am facing occasional chip reset or very rare chip hanging.

    This topic has been closed for replies.